Hi,
I've looked through previous posting regarding get splash screens in uboot. All seems to indicate that
you need to add:
#define CONFIG_SPLASH_SCREEN
to your board config file.
I've added the line above to the file:
include/configs/am335x_evm.h
After compile, Im expecting the bmp command to be available in uboot
but it isnt.
If I add:
#define_cmd_bmp
to the same file the common/cmd_bmp.c gets compiled but
as other have mentioned you have to define
#define CONFIG_LCD/CONFIG_VIDEO
I want the splash screen to appear on the hmdi initially but later on lcd.
If I define either I get errors for missing symbols:
lcd_setcolreg
panel_info
etc
Ive tried with uboot version 15.07-00001 and the version which comes with the sdk,
but fail in same way!
Can some help, as its clear that others are getting this to work!?!