Hi,
i did not see any specific instructions in the wiki
http://processors.wiki.ti.com/index.php/Linux_Core_U-Boot_User%27s_Guide#Building_MLO_and_u-boot
for a QSPI NOR XIP boot for the AM437x Starterkit EVM.
But here is what I am thinking:
[] build u-boot with host# make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- am43xx_evm_qspiboot_config
[] output will be u-boot.img and u-boot.bin
[] need to flash one of those binaries into QSPI NOR at offset 0
[] then it should boot from qspi nor with execute in place
Can someone confirm that this is correct?
What binary needs to be flashed into the QSPI NOR exactly? Can you share the exact u-boot cmds just so there is no question about the flashing?
Thanks,
--Gunter