Hi,
Since using .dtb file, I find that TFTP boot and remote NFS always have problem on Sitara AM3359 SK board.
I do not success to generate uboot.env yet. uEnv.txt is still used now. Its content is:
serverip=192.168.0.109
ipaddr=192.168.0.112
loadaddr=0x82000000
rootpath=/home/u64rj/ti-processor-sdk-linux-am335x-evm-01.00.00.03/targetNFS
bootfile=zImage
ip_method=dhcp
autoload=no
bootdelay=5
tftp_nfs_boot=run findfdt; setenv autoload no;dhcp; tftp 0x82000000 am335x-evmsk.dtb; run findfdt; tftp tftp 0x82d80000 am335x-evmsk.dtb; run netargs; bootz 0x82000000 - 0x82d80000
uenvcmd=run tftp_nfs_boot
The boot message is below. It looks like TFTP the kernel succeeds, but TFTP NFS fails. Is it right?
At the end of the message, it shows:
root@am335x-evm:~# cat /proc/cmdline
console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait
Does it only mean that NFS is at mmc memory? It does not say where the kernel is from?
Thanks,
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
403 bytes read in 4 ms (97.7 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc ...
Running uenvcmd ...
cpsw Waiting for PHY auto negotiation to complete. done
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
DHCP client bound to address 192.168.0.112
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.0.109; our IP address is 192.168.0.112
Filename 'am335x-evmsk.dtb'.
Load address: 0x82000000
Loading: ########
1.4 MiB/s
done
Bytes transferred = 36445 (8e5d hex)
tftpboot - boot image via network using TFTP protocol
Usage:
tftpboot [loadAddress] [[hostIPaddr:]bootfilename]
Bad Linux ARM zImage magic!
4337552 bytes read in 321 ms (12.9 MiB/s)
36445 bytes read in 58 ms (613.3 KiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x422f90 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8e713000, end 8e71ee5c ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 3.14.43-g875c69b (gtbldadm@ubuntu-12) (gcc version 4.7.3 20130226 (prerelease) (crossto
ol-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #1 Mon Jul 6 16:00:11 EDT 2015
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM-SK
[ 0.000000] cma: CMA: reserved 24 MiB at 8c800000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64768
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 225284K/261120K available (5843K kernel code, 303K rwdata, 2144K rodata, 260K init, 232K bss,
35836K reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc07d50c4 (7989 kB)
[ 0.000000] .init : 0xc07d6000 - 0xc0817144 ( 261 kB)
[ 0.000000] .data : 0xc0818000 - 0xc0863da0 ( 304 kB)
[ 0.000000] .bss : 0xc0863da0 - 0xc089ddb8 ( 233 kB)
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns
[ 0.000038] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000334] Console: colour dummy device 80x30
[ 0.000362] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000368] This ensures that you still see kernel messages. Please
[ 0.000374] update your kernel commandline.
[ 0.000399] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.119360] pid_max: default: 32768 minimum: 301
[ 0.119463] Security Framework initialized
[ 0.119524] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.119535] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.127616] CPU: Testing write buffer coherency: ok
[ 0.128021] Setting up static identity map for 0x805baa20 - 0x805baa78
[ 0.129049] devtmpfs: initialized
[ 0.131074] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.138972] omap_hwmod: tptc0 using broken dt data from edma
[ 0.139060] omap_hwmod: tptc1 using broken dt data from edma
[ 0.139140] omap_hwmod: tptc2 using broken dt data from edma
[ 0.143516] omap_hwmod: debugss: _wait_target_disable failed
[ 0.199570] pinctrl core: initialized pinctrl subsystem
[ 0.200680] regulator-dummy: no parameters
[ 0.203199] NET: Registered protocol family 16
[ 0.205394] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.208165] cpuidle: using governor ladder
[ 0.208184] cpuidle: using governor menu
[ 0.215212] syscon 44e10000.control_module: regmap [mem 0x44e10000-0x44e107fb] registered
[ 0.216794] platform 49000000.edma: alias fck already exists
[ 0.216821] platform 49000000.edma: alias fck already exists
[ 0.216836] platform 49000000.edma: alias fck already exists
[ 0.218041] OMAP GPIO hardware version 0.1
[ 0.233550] No ATAGs?
[ 0.233574] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.262486] bio: create slab <bio-0> at 0
[ 0.280019] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.281126] vbat: 5000 mV
[ 0.281539] lis3_reg: no parameters
[ 0.281652] reg-fixed-voltage fixedregulator@2: could not find pctldev for node /pinmux@44e10800/pinmux_wl12xx_gp
io, deferring probe
[ 0.281678] platform fixedregulator@2: Driver reg-fixed-voltage requests probe deferral
[ 0.282144] vtt: 1500 mV
[ 0.285547] vgaarb: loaded
[ 0.286118] i2c-core: driver [palmas] using legacy suspend method
[ 0.286130] i2c-core: driver [palmas] using legacy resume method
[ 0.286898] SCSI subsystem initialized
[ 0.288519] usbcore: registered new interface driver usbfs
[ 0.288723] usbcore: registered new interface driver hub
[ 0.288942] usbcore: registered new device driver usb
[ 0.290046] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c0_pins, deferring p
robe
[ 0.290078] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral
[ 0.290522] pps_core: LinuxPPS API ver. 1 registered
[ 0.290534] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.290676] PTP clock support registered
[ 0.292797] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.293755] Advanced Linux Sound Architecture Driver Initialized.
[ 0.295479] Switched to clocksource timer1
[ 0.316770] NET: Registered protocol family 2
[ 0.317698] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.317736] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.317767] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.317838] TCP: reno registered
[ 0.317852] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.317874] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.318059] NET: Registered protocol family 1
[ 0.318481] RPC: Registered named UNIX socket transport module.
[ 0.318493] RPC: Registered udp transport module.
[ 0.318501] RPC: Registered tcp transport module.
[ 0.318508] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.319660] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available
[ 0.322575] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.508935] VFS: Disk quotas dquot_6.5.2
[ 0.509007] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.509563] NFS: Registering the id_resolver key type
[ 0.509643] Key type id_resolver registered
[ 0.509652] Key type id_legacy registered
[ 0.509694] jffs2: version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc.
[ 0.509885] msgmni has been set to 488
[ 0.511465] NET: Registered protocol family 38
[ 0.511511] io scheduler noop registered
[ 0.511520] io scheduler deadline registered
[ 0.511545] io scheduler cfq registered (default)
[ 0.513477] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.517749] backlight supply power not found, using dummy regulator
[ 0.521731] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.527586] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a 8250
[ 1.181938] console [ttyS0] enabled
[ 1.187491] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 1.194549] [drm] Initialized drm 1.1.0 20060810
[ 1.211001] brd: module loaded
[ 1.220190] loop: module loaded
[ 1.223775] (hci_tty): inside hci_tty_init
[ 1.228476] (hci_tty): allocated 250, 0
[ 1.236962] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.247675] usbcore: registered new interface driver asix
[ 1.253340] usbcore: registered new interface driver ax88179_178a
[ 1.259662] usbcore: registered new interface driver cdc_ether
[ 1.265758] usbcore: registered new interface driver smsc95xx
[ 1.271726] usbcore: registered new interface driver net1080
[ 1.277583] usbcore: registered new interface driver cdc_subset
[ 1.283715] usbcore: registered new interface driver zaurus
[ 1.289545] usbcore: registered new interface driver cdc_ncm
[ 1.295835] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.302395] ehci-pci: EHCI PCI platform driver
[ 1.307095] ehci-omap: OMAP-EHCI Host Controller driver
[ 1.312875] usbcore: registered new interface driver cdc_wdm
[ 1.318813] usbcore: registered new interface driver usb-storage
[ 1.326043] mousedev: PS/2 mouse device common for all mice
[ 1.333475] input: ti-tsc as /devices/ocp/44e0d000.tscadc/TI-am335x-tsc/input/input0
[ 1.342862] i2c-core: driver [rtc-ds1307] using legacy suspend method
[ 1.349385] i2c-core: driver [rtc-ds1307] using legacy resume method
[ 1.356619] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 1.363740] 44e3e000.rtc: already running
[ 1.368708] i2c /dev entries driver
[ 1.372397] Driver for 1-wire Dallas network protocol.
[ 1.380245] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.389320] omap_hsmmc 48060000.mmc: unable to get vmmc regulator -517
[ 1.396169] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral
[ 1.403594] omap_hsmmc 481d8000.mmc: unable to get vmmc regulator -517
[ 1.410284] platform 481d8000.mmc: Driver omap_hsmmc requests probe deferral
[ 1.419703] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.426160] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 1.433319] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 1.440796] usbcore: registered new interface driver usbhid
[ 1.446442] usbhid: USB HID core driver
[ 1.450592] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 1.461226] oprofile: using arm/armv7
[ 1.465239] TCP: cubic registered
[ 1.468639] Initializing XFRM netlink socket
[ 1.473021] NET: Registered protocol family 17
[ 1.477559] NET: Registered protocol family 15
[ 1.482136] Key type dns_resolver registered
[ 1.487240] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
[ 1.496040] cpu cpu0: cpu0 clock notifier not ready, retry
[ 1.501648] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
[ 1.509800] PM: bootloader does not support rtc-only!
[ 1.514889] ThumbEE CPU extension supported.
[ 1.519335] Registering SWP/SWPB emulation handler
[ 1.525872] lis3_reg: disabling
[ 1.529037] vbat: disabling
[ 1.531841] regulator-dummy: disabling
[ 1.536452] Error: Driver 'tfp410' is already registered, aborting...
[ 1.545585] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.552237] [drm] No driver support for vblank timestamp query.
[ 1.608019] Console: switching to colour frame buffer device 60x34
[ 1.616611] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.622209] tilcdc 4830e000.lcdc: registered panic notifier
[ 1.627840] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.634971] vwl1271: 1800 mV
[ 1.640139] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.650576] vrtc: 1800 mV
[ 1.653586] vrtc: supplied by vbat
[ 1.658835] vio: at 1500 mV
[ 1.661816] vio: supplied by vbat
[ 1.667035] vdd_mpu: 912 <--> 1375 mV at 1137 mV
[ 1.671843] vdd_mpu: supplied by vbat
[ 1.677421] vdd_core: 912 <--> 1150 mV at 1137 mV
[ 1.682328] vdd_core: supplied by vbat
[ 1.687629] vdd3: 5000 mV
[ 1.691762] vdig1: at 1800 mV
[ 1.694921] vdig1: supplied by vbat
[ 1.699892] vdig2: at 1800 mV
[ 1.703042] vdig2: supplied by vbat
[ 1.707988] vpll: at 1800 mV
[ 1.711046] vpll: supplied by vbat
[ 1.715940] vdac: at 1800 mV
[ 1.719000] vdac: supplied by vbat
[ 1.723806] vaux1: at 1800 mV
[ 1.726983] vaux1: supplied by vbat
[ 1.731928] vaux2: at 3300 mV
[ 1.735082] vaux2: supplied by vbat
[ 1.740026] vaux33: at 3300 mV
[ 1.743252] vaux33: supplied by vbat
[ 1.748259] vmmc: 1800 <--> 3300 mV at 3300 mV
[ 1.752876] vmmc: supplied by vbat
[ 1.758253] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.886352] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 1.899871] mmc0: new high speed SDHC card at address aaaa
[ 1.906290] mmcblk0: mmc0:aaaa SU04G 3.69 GiB
[ 1.914571] mmcblk0: p1 p2
[ 1.926268] remoteproc0: wkup_m3 is available
[ 1.930748] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 1.939798] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed
.
[ 1.950416] remoteproc0: Direct firmware load failed with error -2
[ 1.956792] remoteproc0: Falling back to user helper
[ 1.962402] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[1100000<->1260000]:-22
[ 1.977832] omap_hsmmc 481d8000.mmc: card claims to support voltages below defined range
[ 2.009808] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[ 2.016206] mmc1: new SDIO card at address 0001
[ 2.045647] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 2.051789] davinci_mdio 4a101000.mdio: detected phy mask fffffffc
[ 2.059512] libphy: 4a101000.mdio: probed
[ 2.063555] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Atheros 8031 ethernet
[ 2.072867] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver Atheros 8031 ethernet
[ 2.083099] cpsw 4a100000.ethernet: Detected MACID = d4:94:a1:86:09:c3
[ 2.091060] cpsw 4a100000.ethernet: cpsw: Detected MACID = d4:94:a1:86:09:c4
[ 2.100683] input: gpio_buttons@0 as /devices/gpio_buttons@0/input/input1
[ 2.108414] omap_rtc 44e3e000.rtc: setting system clock to 2015-07-07 14:19:46 UTC (1436278786)
[ 2.120512] ALSA device list:
[ 2.123514] No soundcards found.
[ 2.145252] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.153527] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[ 2.166559] devtmpfs: mounted
[ 2.170010] Freeing unused kernel memory: 260K (c07d6000 - c0817000)
INIT: version 2.88 booting
Starting udev
[ 3.116037] udevd[877]: starting version 182
[ 3.573186] remoteproc0: powering up wkup_m3
[ 3.599243] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 154412
[ 3.692058] PM: CM3 Firmware Version = 0x190
[ 3.696645] lis3lv02d: 16 bits lis331dlh sensor found
[ 3.742413] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 3.771729] remoteproc0: remote processor wkup_m3 is now up
[ 3.810928] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 3.846024] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input2
[ 3.867884] cryptodev: driver 1.6 loaded.
[ 4.244021] EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered
[ 4.336292] Loading modules backported from Linux version R8.5-2-gad69b45
[ 4.343147] Backport generated by backports.git R8.4-0-g0d46f43
Starting Bootlog daemon: [ 4.714261] wl1271_sdio mmc1:0001:2: No platform data set
[ 4.765682] wl1271_sdio: probe of mmc1:0001:2 failed with error -12
bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
[ 5.119110] random: dd urandom read with 103 bits of entropy available
[ 5.196906] davinci_evm sound: tlv320aic3x-hifi <-> 4803c000.mcasp mapping ok
[ 6.340826] musb-hdrc musb-hdrc.0.auto: MUSB HDRC host driver
udevadm settle - timeout of 3 seconds reached, the event queue contains:
/sys/devices/ocp/48060000.mmc/mmc_host/mmc0/mmc0:aaaa/block/mmcblk0/mmcblk0p1 (852)
/sys/devices/ocp/48060000.mmc/mmc_host/mmc0/mmc0:aaaa/block/mmcblk0/mmcblk0p2 (853)
/sys/devices/virtual/block/ram0 (1008)
/sys/devices/virtual/block/ram1 (1009)
/sys/devices/virtual/block/ram10 (1010)
/sys/devices/virtual/block/ram11 (1011)
/sys/devices/virtual/block/ram12 (1012)
/sys/devices/virtual/block/ram13 (1013)
/sys/devices/virtual/block/ram14 (1014)
/sys/devices/virtual/block/ram15 (1015)
/sys/devices/virtual/block/ram2 (1016)
/sys/devices/virtual/block/ram3 (1017)
/sys/devices/virtual/block/ram4 (1018)
/sys/devices/virtual/block/ram5 (1019)
/sys/devices/virtual/block/ram6 (1020)
/sys/devices/virtual/block/ram7 (1021)
/sys/devices/virtual/block/ram8 (1022)
/sys/devices/virtual/block/ram9 (1023)
/sys/devices/virtual/net/lo (1030)
/sys/devices/ocp/47400000.usb/47401400.usb (1046)
/sys/devices/platform/lis3lv02d/input/input2 (1048)
/sys/devices/o[ 6.726161] musb-hdrc musb-hdrc.0.auto: new USB bus registered, assigned bus number 1
cp/47400000.usb/47401c00.usb (1051)
/sys/devices/ocp/47400000.usb/47400000.dma-controller/dma/dma1chan8 (1061)
[ 7.025623] random: nonblocking pool is initialized
[ 7.105926] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 7.112770] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 7.120086] usb usb1: Product: MUSB HDRC host driver
[ 7.125075] usb usb1: Manufacturer: Linux 3.14.43-g875c69b musb-hcd
[ 7.131386] usb usb1: SerialNumber: musb-hdrc.0.auto
[ 7.303066] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 7.377222] hub 1-0:1.0: USB hub found
[ 7.423868] hub 1-0:1.0: 1 port detected
[ 7.470282] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 7.526543] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2
[ 7.584816] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 7.591749] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 7.599042] usb usb2: Product: MUSB HDRC host driver
[ 7.604031] usb usb2: Manufacturer: Linux 3.14.43-g875c69b musb-hcd
[ 7.610344] usb usb2: SerialNumber: musb-hdrc.1.auto
[ 7.650352] hub 2-0:1.0: USB hub found
[ 7.661662] hub 2-0:1.0: 1 port detected
ALSA: Restoring mixer settings...
INIT: Entering runlevel: 5
Configuring network interfaces... [ 8.508213] net eth0: initializing cpsw version 1.12 (0)
[ 8.596291] net eth0: phy found : id is : 0x4dd074
udhcpc (v1.22.1) started
Sending discover...
[ 11.596411] libphy: 4a101000.mdio:00 - Link is Up - 100/Full
Sending discover...
Sending select for 192.168.0.112...
Lease of 192.168.0.112 obtained, lease time 604800
/etc/udhcpc.d/50default: Adding DNS 192.168.0.1
done.
Starting system message bus: dbus.
UIM SYSFS Node Not Found
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting rpcbind daemon...rpcbind: cannot create socket for udp6
rpcbind: cannot create socket for tcp6
done.
creating NFS state directory: done
starting statd: done
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
Starting Lighttpd Web Server: lighttpd.
2015-07-07 14:19:57: (/home/gtbldadm/ti/oe-layersetup/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortex
a8t2hf-vfp-neon-linux-gnueabi/lighttpd/1.4.33-r1/lighttpd-1.4.33/src/log.c.166) server started
/
Starting Matrix GUI application.
Enabling thermal zones...
/etc/rc5.d/S98thermal-zone-init: line 7: /sys/class/thermal/thermal_zone*/mode: No such file or directory
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
autoconf
binutils
cpp-symlinks
cpp
g++-symlinks
g++
gcc-symlinks
gcc
gdbserver
gstreamer1.0-libav
libgmp10
libmpc3
libmpfr4
make
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm /dev/ttyO0
Arago 2015.05 am335x-evm /dev/ttyO0
am335x-evm login: root
root@am335x-evm:~# cat /proc/cmdline
console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait
root@am335x-evm:~#