Hi,
Just bought this kit for evaluation. I'm trying to use hardware acceleration for ssl (AES128-SHA cipher).
I've seen that there was an issue with SHA acceleration, was it fixed?
I'm using ti-sdk-am335x-evm-06.00.00
I've created self signed certificate and run on board
openssl s_server -accept 4000 -cert ./root.crt -key ./root.key
if I run openssl s_client -connect 192.168.10.87:4000 -cipher AES128-SHA from the same board it works as expected.
but if I run openssl s_client -connect 192.168.10.87:4000 -cipher AES128-SHA from pc linux computer then I get
ACCEPT
ERROR
1074476768:error:1408F119:SSL routines:SSL3_GET_RECORD:decryption failed or bad record mac:s3_pkt.c:479:
shutting down SSL
CONNECTION CLOSED
ACCEPT
Thank you for your help.