Hi All,
We have a custom board based on AM3352, and the boot sequence is as follows.
I have 2MB SPI flash, where in I have MLO & u-boot
I want to save kernel & filesystem on NAND.
1) I am able to detect NAND in u-boot
U-Boot# nand info
Device 0: nand0, sector size 128 KiB
Page size 2048 b
OOB size 64 b
Erase size 131072 b
subpagesize 512 b
options 0x c
bbt options 0x 8000
2) I am unable to find nandecc command, is it mandatory to set the ecc type?
3) My NAND layout contains kernel & filesystem, kernel starting from 0x0 to 0x500000, Booting from uSD I am able to write kernel Image to NAND
Kernel version I have is 3.8 & using dts, so what is the Kernel Image I have to use, whether uImage or uImage-dtb.bone-black ?
When I used uImage-dtb.bone-black, it starts booting and stops after the print "Uncompressing Linux... done, booting the kernel."
When I used uImage I see the following message.
U-Boot SPL 2015.07-00260-g7757405-dirty (Oct 07 2015 - 21:17:31)
reading u-boot.img
reading u-boot.img
U-Boot 2015.07-00260-g7757405-dirty (Oct 07 2015 - 21:17:31 +0530)
Watchdog enabled
I2C: ready
DRAM: 256 MiB
NAND: 1024 MiB
MMC: OMAP SD/MMC: 0
SF: Detected M25P16 with page size 256 Bytes, erase size 64 KiB, total 2 MiB
Net: cpsw
Hit any key to stop autoboot: 0
U-Boot# nand read ${loadaddr} 0x0 0x500000
NAND read: device 0 offset 0x0, size 0x500000
5242880 bytes read: OK
U-Boot# bootm ${loadaddr}
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-3.8.13-00774-g18e2dc2
Created: 2015-10-12 6:58:20 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4363160 Bytes = 4.2 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Error: unrecognized/unsupported machine ID (r1 = 0x00000e05).
Available machine support:
ID (hex) NAME
ffffffff Generic OMAP4 (Flattened Device Tree)
ffffffff Generic AM33XX (Flattened Device Tree)
ffffffff Generic OMAP3-GP (Flattened Device Tree)
ffffffff Generic OMAP3 (Flattened Device Tree)
0000060a OMAP3 Beagle Board
00000a9d IGEP OMAP3 module
00000928 IGEP v2 board
00000ae7 OMAP4 Panda board
Please check your kernel config and/or bootloader.
Please give information which type of kernle Image I have to write to NAND, should I need to keep another copy of kernel Image ??
How to add NAND device & partitions in kernel dts file, so that it is detected by kernle?
Please help at the earliest.
Thanks & Regards,
gvk51.