Hello,
Can anyone please highlight major differences between AM335x Rev 1.4A and AM335x rev 1.5C?? Where can i find the documents regarding new rev 1.5C??
Thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can anyone please highlight major differences between AM335x Rev 1.4A and AM335x rev 1.5C?? Where can i find the documents regarding new rev 1.5C??
Thanks in advance
Is there a way to find on the fly (During code execution) that which SDRAM (DDR2 or DDR3) is installed?
In U-Boot source.. There is a way to determine which memory configuration needs to be set
This is in <U-Boot Source>board\ti\am335x\board.c
Line # 459
if (board_is_evm_sk(&header)) config_ddr(303, &ioregs_evmsk, &ddr3_data, &ddr3_cmd_ctrl_data, &ddr3_emif_reg_data, 0); else if (board_is_bone_lt(&header)) config_ddr(400, &ioregs_bonelt, &ddr3_beagleblack_data, &ddr3_beagleblack_cmd_ctrl_data, &ddr3_beagleblack_emif_reg_data, 0); else if (board_is_evm_15_or_later(&header)) config_ddr(303, &ioregs_evm15, &ddr3_evm_data, &ddr3_evm_cmd_ctrl_data, &ddr3_evm_emif_reg_data, 0); else config_ddr(266, &ioregs, &ddr2_data, &ddr2_cmd_ctrl_data, &ddr2_emif_reg_data, 0);