Hi Team,
We are having AM5728 based custom board (We used DRA7Xx EVM rev G as reference for schematics), occasionaly we see the mtest in the u-boot fails. We are using the following DDR3:
1. MT41K256M8DA-125
2. MT41K128M16JT-125
similar what is there in the DRA7xx EVM, the orgnisation is same as EVM like 512MB is on EMIF1 and 1 GB on EMIF2.
The trace lengths are attached. The timings that are used are as given in the board file attached.
The kernel stops at starting Kernel .................. We are using the Processor SDK 2.0 and made relevant changes in the MLO/u-boot for pinux and the uart support.
Since it some times fails with the mtest we suspect it should be DDR3 issue, could you please provide pointers, review the timing values and help solve the issue Tracelengths.pdf
/* * Copyright (C) 2014 Texas Instruments Incorporated - http://www.ti.com * * Author: Felipe Balbi <balbi@ti.com> * * Based on board/ti/dra7xx/evm.c * * SPDX-License-Identifier: GPL-2.0+ */ #include <common.h> #include <palmas.h> #include <sata.h> #include <usb.h> #include <asm/omap_common.h> #include <asm/emif.h> #include <asm/gpio.h> #include <asm/arch/gpio.h> #include <asm/arch/clock.h> #include <asm/arch/dra7xx_iodelay.h> #include <asm/arch/sys_proto.h> #include <asm/arch/mmc_host_def.h> #include <asm/arch/sata.h> #include <asm/arch/gpio.h> #include <asm/arch/omap.h> #include <environment.h> #include <usb.h> #include <linux/usb/gadget.h> #include <dwc3-uboot.h> #include <dwc3-omap-uboot.h> #include <ti-usb-phy-uboot.h> #include "mux_data.h" #ifdef CONFIG_DRIVER_TI_CPSW #include <cpsw.h> #endif DECLARE_GLOBAL_DATA_PTR; /* GPIO 7_11 */ #define GPIO_DDR_VTT_EN 203 const struct omap_sysinfo sysinfo = { "Board: BeagleBoard x15\n" }; static const struct dmm_lisa_map_regs beagle_x15_lisa_regs = { .dmm_lisa_map_0 = 0x0, .dmm_lisa_map_1 = 0x80640300, .dmm_lisa_map_2 = 0xC0500220, .dmm_lisa_map_3 = 0xFF020100, .is_ma_present = 0x1 }; void emif_get_dmm_regs(const struct dmm_lisa_map_regs **dmm_lisa_regs) { *dmm_lisa_regs = &beagle_x15_lisa_regs; } static const struct emif_regs beagle_x15_emif1_ddr3_532mhz_emif_regs = { #if 0 .sdram_config_init = 0x61851b32, .sdram_config = 0x61851b32, .sdram_config2 = 0x00000000, .ref_ctrl = 0x000040F1, .ref_ctrl_final = 0x00001035, .sdram_tim1 = 0xceef266b, .sdram_tim2 = 0x328f7fda, .sdram_tim3 = 0x027f88a8, .read_idle_ctrl = 0x00050000, .zq_config = 0x0007190b, .temp_alert_config = 0x00000000, .emif_ddr_phy_ctlr_1_init = 0x0024400b, .emif_ddr_phy_ctlr_1 = 0x0e24400b, .emif_ddr_ext_phy_ctrl_1 = 0x10040100, .emif_ddr_ext_phy_ctrl_2 = 0x00740074, .emif_ddr_ext_phy_ctrl_3 = 0x00780078, .emif_ddr_ext_phy_ctrl_4 = 0x007c007c, .emif_ddr_ext_phy_ctrl_5 = 0x007b007b, .emif_rd_wr_lvl_rmp_win = 0x00000000, .emif_rd_wr_lvl_rmp_ctl = 0x80000000, .emif_rd_wr_lvl_ctl = 0x00000000, .emif_rd_wr_exec_thresh = 0x00000305 #endif .sdram_config_init = 0x61851ab2, .sdram_config = 0x61851ab2, .sdram_config2 = 0x08000000, .ref_ctrl = 0x000040F1, .ref_ctrl_final = 0x00001035, .sdram_tim1 = 0xCCCF36B3, .sdram_tim2 = 0x308F7FDA, .sdram_tim3 = 0x027F88A8, .read_idle_ctrl = 0x00050000, .zq_config = 0x0007190B, .temp_alert_config = 0x00000000, //.emif_ddr_phy_ctlr_1_init = 0x0E24400A, //.emif_ddr_phy_ctlr_1 = 0x0E24400A, .emif_ddr_phy_ctlr_1_init = 0x0024400B, .emif_ddr_phy_ctlr_1 = 0x0E24400B, .emif_ddr_ext_phy_ctrl_1 = 0x10040100, .emif_ddr_ext_phy_ctrl_2 = 0x00910091, .emif_ddr_ext_phy_ctrl_3 = 0x00950095, .emif_ddr_ext_phy_ctrl_4 = 0x009B009B, .emif_ddr_ext_phy_ctrl_5 = 0x009E009E, .emif_rd_wr_lvl_rmp_win = 0x00000000, //.emif_rd_wr_lvl_rmp_ctl = 0x00000000, .emif_rd_wr_lvl_rmp_ctl = 0x80000000, .emif_rd_wr_lvl_ctl = 0x00000000, .emif_rd_wr_exec_thresh = 0x00000305 }; /* Ext phy ctrl regs 1-35 */ static const u32 beagle_x15_emif1_ddr3_ext_phy_ctrl_const_regs[] = { #if 0 0x10040100, 0x00740074, 0x00780078, 0x007c007c, 0x007b007b, 0x00800080, 0x00360036, 0x00340034, 0x00360036, 0x00350035, 0x00350035, 0x01ff01ff, 0x01ff01ff, 0x01ff01ff, 0x01ff01ff, 0x01ff01ff, 0x00430043, 0x003e003e, 0x004a004a, 0x00470047, 0x00400040, 0x00000000, 0x00600020, 0x40011080, 0x08102040, 0x00400040, 0x00400040, 0x00400040, 0x00400040, 0x00400040, 0x0, 0x0, 0x0, 0x0, 0x0 #endif 0x10040100, 0x00910091, 0x00950095, 0x009B009B, 0x009E009E, 0x00980098, 0x00340034, 0x00350035, 0x00340034, 0x00310031, 0x00340034, 0x007F007F, 0x007F007F, 0x007F007F, 0x007F007F, 0x007F007F, 0x00480048, 0x004A004A, 0x00520052, 0x00550055, 0x00500050, 0x00000000, 0x00600020, 0x40011080, 0x08102040, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0 }; static const struct emif_regs beagle_x15_emif2_ddr3_532mhz_emif_regs = { #if 0 .sdram_config_init = 0x61851b32, .sdram_config = 0x61851b32, .sdram_config2 = 0x00000000, .ref_ctrl = 0x000040F1, .ref_ctrl_final = 0x00001035, .sdram_tim1 = 0xceef266b, .sdram_tim2 = 0x328f7fda, .sdram_tim3 = 0x027f88a8, .read_idle_ctrl = 0x00050000, .zq_config = 0x0007190b, .temp_alert_config = 0x00000000, .emif_ddr_phy_ctlr_1_init = 0x0024400b, .emif_ddr_phy_ctlr_1 = 0x0e24400b, .emif_ddr_ext_phy_ctrl_1 = 0x10040100, .emif_ddr_ext_phy_ctrl_2 = 0x00820082, .emif_ddr_ext_phy_ctrl_3 = 0x008b008b, .emif_ddr_ext_phy_ctrl_4 = 0x00800080, .emif_ddr_ext_phy_ctrl_5 = 0x007e007e, .emif_rd_wr_lvl_rmp_win = 0x00000000, .emif_rd_wr_lvl_rmp_ctl = 0x80000000, .emif_rd_wr_lvl_ctl = 0x00000000, .emif_rd_wr_exec_thresh = 0x00000305 #endif .sdram_config_init = 0x61851B32, .sdram_config = 0x61851B32, .sdram_config2 = 0x08000000, .ref_ctrl = 0x000040F1, .ref_ctrl_final = 0x00001035, .sdram_tim1 = 0xCCCF36B3, .sdram_tim2 = 0x308F7FDA, .sdram_tim3 = 0x027F88A8, .read_idle_ctrl = 0x00050000, .zq_config = 0x0007190B, .temp_alert_config = 0x00000000, //.emif_ddr_phy_ctlr_1_init = 0x0E24400A, //.emif_ddr_phy_ctlr_1 = 0x0E24400A, .emif_ddr_phy_ctlr_1_init = 0x0024400B, .emif_ddr_phy_ctlr_1 = 0x0E24400B, .emif_ddr_ext_phy_ctrl_1 = 0x10040100, .emif_ddr_ext_phy_ctrl_2 = 0x00910091, .emif_ddr_ext_phy_ctrl_3 = 0x00950095, .emif_ddr_ext_phy_ctrl_4 = 0x009B009B, .emif_ddr_ext_phy_ctrl_5 = 0x009E009E, .emif_rd_wr_lvl_rmp_win = 0x00000000, //.emif_rd_wr_lvl_rmp_ctl = 0x00000000, .emif_rd_wr_lvl_rmp_ctl = 0x80000000, .emif_rd_wr_lvl_ctl = 0x00000000, .emif_rd_wr_exec_thresh = 0x00000305 }; static const u32 beagle_x15_emif2_ddr3_ext_phy_ctrl_const_regs[] = { #if 0 0x10040100, 0x00820082, 0x008b008b, 0x00800080, 0x007e007e, 0x00800080, 0x00370037, 0x00390039, 0x00360036, 0x00370037, 0x00350035, 0x01ff01ff, 0x01ff01ff, 0x01ff01ff, 0x01ff01ff, 0x01ff01ff, 0x00540054, 0x00540054, 0x004e004e, 0x004c004c, 0x00400040, 0x00000000, 0x00600020, 0x40011080, 0x08102040, 0x00400040, 0x00400040, 0x00400040, 0x00400040, 0x00400040, 0x0, 0x0, 0x0, 0x0, 0x0 #endif 0x10040100, 0x00910091, 0x00950095, 0x009B009B, 0x009E009E, 0x00980098, 0x00340034, 0x00350035, 0x00340034, 0x00310031, 0x00340034, 0x007F007F, 0x007F007F, 0x007F007F, 0x007F007F, 0x007F007F, 0x00480048, 0x004A004A, 0x00520052, 0x00550055, 0x00500050, 0x00000000, 0x00600020, 0x40011080, 0x08102040, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0 }; void emif_get_reg_dump(u32 emif_nr, const struct emif_regs **regs) { switch (emif_nr) { case 1: *regs = &beagle_x15_emif1_ddr3_532mhz_emif_regs; break; case 2: *regs = &beagle_x15_emif2_ddr3_532mhz_emif_regs; break; } } void emif_get_ext_phy_ctrl_const_regs(u32 emif_nr, const u32 **regs, u32 *size) { switch (emif_nr) { case 1: *regs = beagle_x15_emif1_ddr3_ext_phy_ctrl_const_regs; *size = ARRAY_SIZE(beagle_x15_emif1_ddr3_ext_phy_ctrl_const_regs); break; case 2: *regs = beagle_x15_emif2_ddr3_ext_phy_ctrl_const_regs; *size = ARRAY_SIZE(beagle_x15_emif2_ddr3_ext_phy_ctrl_const_regs); break; } } struct vcores_data beagle_x15_volts = { .mpu.value = VDD_MPU_DRA752, .mpu.efuse.reg = STD_FUSE_OPP_VMIN_MPU_NOM, .mpu.efuse.reg_bits = DRA752_EFUSE_REGBITS, .mpu.addr = TPS659038_REG_ADDR_SMPS12, .mpu.pmic = &tps659038, .eve.value = VDD_EVE_DRA752, .eve.efuse.reg = STD_FUSE_OPP_VMIN_DSPEVE_NOM, .eve.efuse.reg_bits = DRA752_EFUSE_REGBITS, .eve.addr = TPS659038_REG_ADDR_SMPS45, .eve.pmic = &tps659038, .gpu.value = VDD_GPU_DRA752, .gpu.efuse.reg = STD_FUSE_OPP_VMIN_GPU_NOM, .gpu.efuse.reg_bits = DRA752_EFUSE_REGBITS, .gpu.addr = TPS659038_REG_ADDR_SMPS6, .gpu.pmic = &tps659038, .core.value = VDD_CORE_DRA752, .core.efuse.reg = STD_FUSE_OPP_VMIN_CORE_NOM, .core.efuse.reg_bits = DRA752_EFUSE_REGBITS, .core.addr = TPS659038_REG_ADDR_SMPS7, .core.pmic = &tps659038, .iva.value = VDD_IVA_DRA752, .iva.efuse.reg = STD_FUSE_OPP_VMIN_IVA_NOM, .iva.efuse.reg_bits = DRA752_EFUSE_REGBITS, .iva.addr = TPS659038_REG_ADDR_SMPS8, .iva.pmic = &tps659038, }; void hw_data_init(void) { *prcm = &dra7xx_prcm; *dplls_data = &dra7xx_dplls; *omap_vcores = &beagle_x15_volts; *ctrl = &dra7xx_ctrl; } int board_init(void) { gpmc_init(); gd->bd->bi_boot_params = (CONFIG_SYS_SDRAM_BASE + 0x100); return 0; } int board_late_init(void) { init_sata(0); /* * DEV_CTRL.DEV_ON = 1 please - else palmas switches off in 8 seconds * This is the POWERHOLD-in-Low behavior. */ palmas_i2c_write_u8(TPS65903X_CHIP_P1, 0xA0, 0x1); return 0; } void set_muxconf_regs_essential(void) { do_set_mux32((*ctrl)->control_padconf_core_base, early_padconf, ARRAY_SIZE(early_padconf)); } #ifdef CONFIG_IODELAY_RECALIBRATION void recalibrate_iodelay(void) { __recalibrate_iodelay(core_padconf_array_essential, ARRAY_SIZE(core_padconf_array_essential), iodelay_cfg_array, ARRAY_SIZE(iodelay_cfg_array)); } #endif #if !defined(CONFIG_SPL_BUILD) && defined(CONFIG_GENERIC_MMC) int board_mmc_init(bd_t *bis) { omap_mmc_init(0, 0, 0, -1, -1); omap_mmc_init(1, 0, 0, -1, -1); return 0; } #endif #if defined(CONFIG_SPL_BUILD) && defined(CONFIG_SPL_OS_BOOT) int spl_start_uboot(void) { /* break into full u-boot on 'c' */ if (serial_tstc() && serial_getc() == 'c') return 1; #ifdef CONFIG_SPL_ENV_SUPPORT env_init(); env_relocate_spec(); if (getenv_yesno("boot_os") != 1) return 1; #endif return 0; } #endif #ifdef CONFIG_USB_DWC3 static struct dwc3_device usb_otg_ss1 = { .maximum_speed = USB_SPEED_SUPER, .base = DRA7_USB_OTG_SS1_BASE, .tx_fifo_resize = false, .index = 0, }; static struct dwc3_omap_device usb_otg_ss1_glue = { .base = (void *)DRA7_USB_OTG_SS1_GLUE_BASE, .utmi_mode = DWC3_OMAP_UTMI_MODE_SW, .index = 0, }; static struct ti_usb_phy_device usb_phy1_device = { .pll_ctrl_base = (void *)DRA7_USB3_PHY1_PLL_CTRL, .usb2_phy_power = (void *)DRA7_USB2_PHY1_POWER, .usb3_phy_power = (void *)DRA7_USB3_PHY1_POWER, .index = 0, }; static struct dwc3_device usb_otg_ss2 = { .maximum_speed = USB_SPEED_HIGH, .base = DRA7_USB_OTG_SS2_BASE, .tx_fifo_resize = false, .index = 1, }; static struct dwc3_omap_device usb_otg_ss2_glue = { .base = (void *)DRA7_USB_OTG_SS2_GLUE_BASE, .utmi_mode = DWC3_OMAP_UTMI_MODE_SW, .index = 1, }; static struct ti_usb_phy_device usb_phy2_device = { .usb2_phy_power = (void *)DRA7_USB2_PHY2_POWER, .index = 1, }; int board_usb_init(int index, enum usb_init_type init) { enable_usb_clocks(index); switch (index) { case 0: if (init == USB_INIT_DEVICE) { printf("port %d can't be used as device\n", index); disable_usb_clocks(index); return -EINVAL; } else { usb_otg_ss1.dr_mode = USB_DR_MODE_HOST; usb_otg_ss1_glue.vbus_id_status = OMAP_DWC3_ID_GROUND; setbits_le32((*prcm)->cm_l3init_usb_otg_ss1_clkctrl, OTG_SS_CLKCTRL_MODULEMODE_HW | OPTFCLKEN_REFCLK960M); } ti_usb_phy_uboot_init(&usb_phy1_device); dwc3_omap_uboot_init(&usb_otg_ss1_glue); dwc3_uboot_init(&usb_otg_ss1); break; case 1: if (init == USB_INIT_DEVICE) { usb_otg_ss2.dr_mode = USB_DR_MODE_PERIPHERAL; usb_otg_ss2_glue.vbus_id_status = OMAP_DWC3_VBUS_VALID; } else { printf("port %d can't be used as host\n", index); disable_usb_clocks(index); return -EINVAL; } ti_usb_phy_uboot_init(&usb_phy2_device); dwc3_omap_uboot_init(&usb_otg_ss2_glue); dwc3_uboot_init(&usb_otg_ss2); break; default: printf("Invalid Controller Index\n"); } return 0; } int board_usb_cleanup(int index, enum usb_init_type init) { switch (index) { case 0: case 1: ti_usb_phy_uboot_exit(index); dwc3_uboot_exit(index); dwc3_omap_uboot_exit(index); break; default: printf("Invalid Controller Index\n"); } disable_usb_clocks(index); return 0; } int usb_gadget_handle_interrupts(int index) { u32 status; status = dwc3_omap_uboot_interrupt_status(index); if (status) dwc3_uboot_handle_interrupt(index); return 0; } #endif #ifdef CONFIG_DRIVER_TI_CPSW /* Delay value to add to calibrated value */ #define RGMII0_TXCTL_DLY_VAL ((0x3 << 5) + 0x8) #define RGMII0_TXD0_DLY_VAL ((0x3 << 5) + 0x8) #define RGMII0_TXD1_DLY_VAL ((0x3 << 5) + 0x2) #define RGMII0_TXD2_DLY_VAL ((0x4 << 5) + 0x0) #define RGMII0_TXD3_DLY_VAL ((0x4 << 5) + 0x0) #define VIN2A_D13_DLY_VAL ((0x3 << 5) + 0x8) #define VIN2A_D17_DLY_VAL ((0x3 << 5) + 0x8) #define VIN2A_D16_DLY_VAL ((0x3 << 5) + 0x2) #define VIN2A_D15_DLY_VAL ((0x4 << 5) + 0x0) #define VIN2A_D14_DLY_VAL ((0x4 << 5) + 0x0) static void cpsw_control(int enabled) { /* VTP can be added here */ } static struct cpsw_slave_data cpsw_slaves[] = { { .slave_reg_ofs = 0x208, .sliver_reg_ofs = 0xd80, .phy_addr = 1, }, { .slave_reg_ofs = 0x308, .sliver_reg_ofs = 0xdc0, .phy_addr = 2, }, }; static struct cpsw_platform_data cpsw_data = { .mdio_base = CPSW_MDIO_BASE, .cpsw_base = CPSW_BASE, .mdio_div = 0xff, .channels = 8, .cpdma_reg_ofs = 0x800, .slaves = 1, .slave_data = cpsw_slaves, .ale_reg_ofs = 0xd00, .ale_entries = 1024, .host_port_reg_ofs = 0x108, .hw_stats_reg_ofs = 0x900, .bd_ram_ofs = 0x2000, .mac_control = (1 << 5), .control = cpsw_control, .host_port_num = 0, .version = CPSW_CTRL_VERSION_2, }; int board_eth_init(bd_t *bis) { int ret; uint8_t mac_addr[6]; uint32_t mac_hi, mac_lo; uint32_t ctrl_val; /* try reading mac address from efuse */ mac_lo = readl((*ctrl)->control_core_mac_id_0_lo); mac_hi = readl((*ctrl)->control_core_mac_id_0_hi); mac_addr[0] = (mac_hi & 0xFF0000) >> 16; mac_addr[1] = (mac_hi & 0xFF00) >> 8; mac_addr[2] = mac_hi & 0xFF; mac_addr[3] = (mac_lo & 0xFF0000) >> 16; mac_addr[4] = (mac_lo & 0xFF00) >> 8; mac_addr[5] = mac_lo & 0xFF; if (!getenv("ethaddr")) { printf("<ethaddr> not set. Validating first E-fuse MAC\n"); if (is_valid_ethaddr(mac_addr)) eth_setenv_enetaddr("ethaddr", mac_addr); } mac_lo = readl((*ctrl)->control_core_mac_id_1_lo); mac_hi = readl((*ctrl)->control_core_mac_id_1_hi); mac_addr[0] = (mac_hi & 0xFF0000) >> 16; mac_addr[1] = (mac_hi & 0xFF00) >> 8; mac_addr[2] = mac_hi & 0xFF; mac_addr[3] = (mac_lo & 0xFF0000) >> 16; mac_addr[4] = (mac_lo & 0xFF00) >> 8; mac_addr[5] = mac_lo & 0xFF; if (!getenv("eth1addr")) { if (is_valid_ethaddr(mac_addr)) eth_setenv_enetaddr("eth1addr", mac_addr); } ctrl_val = readl((*ctrl)->control_core_control_io1) & (~0x33); ctrl_val |= 0x22; writel(ctrl_val, (*ctrl)->control_core_control_io1); ret = cpsw_register(&cpsw_data); if (ret < 0) printf("Error %d registering CPSW switch\n", ret); return ret; } #endif #ifdef CONFIG_BOARD_EARLY_INIT_F /* VTT regulator enable */ static inline void vtt_regulator_enable(void) { if (omap_hw_init_context() == OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL) return; gpio_request(GPIO_DDR_VTT_EN, "ddr_vtt_en"); gpio_direction_output(GPIO_DDR_VTT_EN, 1); } int board_early_init_f(void) { vtt_regulator_enable(); return 0; } #endif
?
Best Regards,
Ganesh