Hi All,
We are having a custom board based on AM5728. We want to use the LCD3 output of this. To use the video pll, I see that the register address of Video PLL Config mentioned in the Linux Processor SDK for AM5728 Version 02.00.00.00 and Techinical Reference Manual Version D (Link: ) is different. The address mentioned in SDK in the file arch/arm/boot/dts/dra74x.dtsi for pll2 is 0x58005300 while the address mentioned in the Section 11.1.5 Display Subsystem Register Manual of TRM for DPLL_VIDEO2 is 0x58009300. Can someone help me with which is the correct value to be used?
Regards,
Abhiroop