I am working on designing a PCIe interface between an AM571x processor and an FPGA. In order to avoid an external oscillator on our board, I plan to use the ljcb_clk pins as outputs to provide the PCIe clock to our FPGA.
Looking at SPRUHZ7, AM571x Technical Reference Manual, Table 26-49 implies that only certain clock frequencies on the CLKINP input to the DPLL_PCIE_REF module are verified to meet PCIe clock jitter requirements. This input is derived from SYS_CLK1, for which the datasheet states can be 19.2, 20, or 27MHz. I had been planning on using a 20MHz system clock; however, this is not listed in Table 26-49. Is this configuration simply supported but not tested (assuming I set the multiplier/dividers accordingly to get the required 100MHz PCIe clock)? Why do the frequency specifications of Table 26-49 not match the allowable options for system clock frequencies?
Thanks.