Hi,
according to the TRM, the ACSPCIE module can be used in TX mode. The ljcb_clk pins are then used as PCIe reference clock output (section 26.4.4.4.3).
If I understand this correctly, the ACSPCIe TX mode can be selected in the register CTRL_CORE_SMA_SW_6 => PCIE_TX_RX_CONTROL.
I'm not sure about how we can activate the TX mode using linux and which additional steps are required to configure internal PCIe clocking.
Do we have to activate TX mode in U-Boot and then configure the clocks using the linux device tree?
Thanks,
Ralf