Hi. I have found a strange behaviour when I send data from an windows 7 FTP client to our small ftp server that is built on the NDK.
Just to be sure that our large application doesn't do something strange, I integrated the code into NIMU_BasicExample_evmAM572x..., with the same result.
When I send a file that has a 2k size everyting looks fine in wireshark.
If I switch to a 4k file I always get one retransmission.
Each time I increase the filesize (double the size) I get more and more retransmissions.
The throughput is realy bad. Any hints what can be wrong.
I attach 3 screendumps, 1, 2k and 32k transfers fron wireshark and corresponding cmd-prompt that was running the ftp client.
I can provide the CCS testcode also.
I'm running the latest NDK _25_00_09 and CCS 6.1.2
Regards