Hi,
I am trying to reconfigure the SDRAM configuration from 166MHz to support the 200MHz SDRAM.
I updated the following:
- CORE_CLK modified from 332MHz to 400MHz
- SDRC parameters: (I obtain the following values from the OMAP35x_DDR_register_calc_tools.xls spreadsheet from TI)
- SDRC_ACTIM_CTRLA_p: 0x7AE1B4C6
- SDRC_ACTIM_CTRLB_p: 0x00021217
- SDRC_RFR_CTRL_p: 0x0005E601
- GPMC parameter for NAND flash where the image resides.
After I made all the changes, the bootloader seems to mostly bootup but with some warning/error regarding the I2C not able to access successfully. However, it till jumps to the image.
As it jumps to the image, the system hang where it's configuring the PMIC(TPS65920), which is I2C as well.
Can you let me know if I am missing anything when I configure the system to support 200MHz SDRAM?
Thanks
Augustine