ll,
we are using latest sdk3.00.00.04 .version and uboot 2016.05 .Actually in our custom board we are using sdcard booting.Initial stage without insert the sdcard into the sdcard slot .we got CCCCC on console. But we are using same ddr and same uart0 and sd card connections used .we compiled u-boot and generated MLO and u-boot.img.Actually in evm schematics didnt use am335x_mmc0_wp not given and not used in u-boot source code. same cd pin connected to the processor in our custom board as well as evm.
Our case wp given .How to configure the wp pin u-boot .
compilation steps:
1.from sdk we compiled
2.make u-boot
it will generate MLO and u-boot.img images .these images copied into the sdcard boot partition..
Sdcard insert into the sdslot .but we cant get any logs on console.can you any body face this issue .help me