Hello, I've recently received a batch of prototype boards whose design I based off of the ICEv2 board and I am having trouble getting the 24MHz crystal to oscillate. It will run for just a second or two when I apply power to the board and then it stops. I've been playing with load capacitors, series resistance and feedback resistance with no luck. Even tried a different crystal. This is my first crack at a design with a TI processor, are there any gotchas that I may be overlooking? To my understanding the crystal should fire right up when power is applied to the chip.
A couple of other notes, the NRESETIN_OUT output pin stays low, I am assuming that this is due to the crystal not running and not the other way around. I also just found that I've pulled the RTC_PWRONRSTn pin up to 3.3V but the datasheet says it should be pulled up to 1.8V. I hope I haven't damaged the chip with this as I haven't been able to find what the damage threshold is for that pin in the datasheet.