Our board could work fine with kernel linux 3.2 and linux 3.12.
After when porting driver to kernel linux 4.1. The board could boot up and mount the file system.
But, could access to the file system, and could not type or input character to debug port (uart0).
log:
Thu Jan 1 01:21:00 UTC 1970
INIT: Entering runlevel: 5
Starting system message bus: [ 8.116494] random: dbus-daemon urandom read with 46 bits of entropy available
Failed to start message bus: Failed to read directory "/etc/dbus-1/system.d": No such file or directory
Starting telnet daemon.
Starting syslogd/klogd: done
Stopping Bootlog daemon: bootlogd.
Then it's like the debug port dead.