I'm trying to start GUI applications with TI Linux rootfs (tisdk-rootfs-image-am335x-evm) with my am335x based board.
my kernel is based on processor-sdk-linux-02.00.02.
I'v compiled the Graphics_SDK from Graphics_SDK_setuplinux_hardfp_5_01_01_02.bin and installed it on my rootfs.
Then I executed /opt/gfxsdkdemos/335x-demo to install kernel and userspace graphics modules, then rebooted my board and the matrix-gui also failed to run.
lsmod show pvrsrvkm is loaded, but not used
root@am335x-evm:~# lsmod | grep pvr
pvrsrvkm 179417 0
root@am335x-evm:~#
omaplfb is not loaded and when I try to load her I got error.
root@am335x-evm:~# modprobe -v omaplfb
insmod /lib/modules/4.1.18-260825-gd652361-dirty/extra/omaplfb.ko
[ 1516.799735] omaplfb: Unknown symbol register_vsync_cb (err 0)
[ 1516.805750] omaplfb: Unknown symbol unregister_vsync_cb (err 0)
modprobe: ERROR: could not insert 'omaplfb': Unknown symbol in module, or unknown parameter (see dmesg)
root@am335x-evm:~#
What do I miss?
Thank you.