Hello,
I want to understand how to configure EMIF_OCP_CONFIG. I saw the following GEL in CCS v6.1.3.
C:\ti\ccsv6\ccs_base\emulation\boards\am571x\gel\AM571x_ddr_config.gel
The register is set below. It means that SYS_THRESH_MAX is 10 and MPU_THRESH_MAX is 5. Each reset value is 7.
OCP_CONFIG = 0x0A500000U;
In this case, does System interface (from L3_MAIN interconnect) take priority over MPU interface (from MPU subsystem) to access DDR3? I think 10 is max value even though the field width is 4-bit. Because Table 15-99 in TRM describes as follow. "The total number of entries in the command FIFO is 10." How can I decide to configure the register? Please give me some advice.
Regards,
Kazu