Hi,
TI
I use the the SDK ti-processor-sdk-linux-am57xx-evm-03.00.00.04 ,which the kernel version is linux4.4.12.I modfiy the arch/arm/boot/dts/am57xx-beagle-x15-common.dtsi like that,because my rtc chip is connect to i2c4 bus.
But it does not work fine---when the power down,the time does not go forward.The hardware is fine,because I use the sdk ti-processor-sdk-linux-am57xx-evm-02.00.02.11,the rtc works fine.
What are the difference between the sdk-03 and sdk-02? it seems that the sdk-03 can update the rtc time through the network.
BR,
vefone