Hi everyone,
I'm facing a boot issue on customer board using AM3351 without EEPROM.
I tried two SDK version SDK1.0.0.3 and SDK2.0.2.11, all use the pre-built images.
While I use the SDK2.0.2.11 pre-built image to boot customer board, there are no any log show off.
However, I use SDK1.0.0.3 pre-built image on the same board, the log will show up and last message said can't read the Magic number.
I can edit source to skip reading EEPROM process to make boot process going on SDK1.0.0.3, but not on the SDK2.0.2.11.
I think the S/W initial sequence is not the same between two SDK version.
Is there anyone can tell me what is going on? And how to fix this issue?
BTW, the same issue is happened on AM437x customer's board.
Best Regards,
Wayne Kuo