Hi,
The problem that there is not is up to 0 with being working, and FSM_BUSY of the ADCSTAT register of the AD conversion becoming 1 when our customer operate the frequency of the TSC_ADC conversion as 3MHz.
When AD conversion fell into an error state, what will the procedure of the return method have?
In Table 12-2 TSC_ADC Clock Signals of TRM of AM335x, ADC_CLK becomes MAX24MHz, but ADC_CLK sets it to 3MHz with the data sheet of AM3352, and it is recommended that sampling rate uses it in typ 200kSPS.
Even if ADC_CLK uses MAX24MHz, will the operation be guaranteed?
AD converts six analog values and is going to store it in FIFO0 and makes a value of STEPCONFIG register Mode Field from step1 to step6 00(one-shot).
Data after six AD conversion should be in FIFO0 when I make each step enable then, but the following difference occurs.
Data after seven conversion may be in FIFO0 when our customer make operating frequency of the AD conversion 3Mhz.
Data after six conversion are in FIFO0 by all means when I make operating frequency of the AD conversion 24Mhz.
Two times of AD conversion seems to be done in spite of one-shot mode one analog value.
Will there be this solution?
Best Regards,
Shigehiro Tsuda