Hi,
I have questions about AM335x PRU ICSS EtherCAT firmware APIs.
The question is about "enhanced link detection".
In following TI wiki page, it said
processors.wiki.ti.com/.../PRU_ICSS_EtherCAT_firmware_API_guide
********************************************************************************
Enhanced link detection /Redundancy support - connect pr1_mii0_rxlink to
LED_LINK/LED_SPEED from PHY
********************************************************************************
In this case, I guess Enhanced link is enabled by setting in bsp_init()API as following:
////////////////////////////////////////////////////////////////
mdioParamsInit.enhancedlink_enable = TIESC_MDIO_RX_LINK_DISABLE;
////////////////////////////////////////////////////////////////
Here is my questions:
Q1. If "Enhanced link detection" is disabled, will "Redundancy" be supported?
Or is "Redundancy" only be supported when enhanced link detection is enabled?
Q2. If EtherPHY have a pin which is corresponding to TLK110 LED_SPEED pin and
connecting to "pr1_mii1_rxlink pin and pr1_mii0_rxlink pin",
is it availabe to use enhanced link detection feature by
enabling "Enhanced link detection" by setting in bsp_init()API?
By the way, the EtherPHY is not TI product.
Q3.If Q3 is available, will it support "Redundancy"?
best regards,
g.f.