Hi,
Please help me in choosing the right IBIS models for SI analysis of certain interfaces whose model selection is not clear from the AM5728 TRM.
1. For AM5728 PCIE_TX/1 has Selector_6 as model name. The actual submodel used should have the right deemphasis settings and voltage level along with speed.
a. I believe speed is HS and voltage is 1.2V
b. However it is not clear of what is the deemphasis setting of PCIE PHY?
- The PCIe PHY registers have deemphasis bit which is set to 1 and is read only. Not sure what is the settings corresponding to this register value.
2. Above holds true for USB 3.0 port of AM572x. Please share more information on the correct IBIS model to be used,
3. For Model Selector_5, the sub-models have Slew rate which can be easily found out from reading pad control registers of a pin. However what is not clear is the parameter IND,10 PERCENT% or 5%. How should one choose the same?
Thanks and would appreciate a quicker response from TI experts.
Regards,
Shareef