Hi,
We are using Phytec module with AM3359 with linux-3.2 kernel.
Everything is OK until recently we apply patch-3.2-rt10.patch.bz2 patch to enable the kernel with real-time capabilities to get 1ms timer.
But, after applying the patch, we are facing problem with the AM3359 network interfaces, both eth0 and eth1 are not responding.
only ping is working initially but not getting response to applications which use network interfaces.
Network interface also hangs immediately when we run iperf tool with default configuration, after iperf test even ping does not work.
Please help us to resolve this issue.
Thanks & Regards,
Prabhakar.