Hello to all,
I'm trying to follow the "PRU training: Hands on Lab" and I'm not able to go over the point 2.9 (JTAG connection). I'm using a BeagleBone black, the Jtag is the XDS100V2. I'm using a CCS6.2 on UBUNTU 16.04.
When I try to run the script "PRU cape init" I obtain this message:
ortxA8: Output: ****** PRU Cape PINMUX is being configured *****
CortxA8: Trouble Writing Memory Block at 0x44e10990 on Page 0 of Length 0x4: (Error -1065 @ 0x3D5A) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.407.3)
PRU_Cape_Init() cannot be evaluated.
Target failed to write 0x44E10990
at *((unsigned int *) 0x44e10990)=(0|5) [PRU_CAPE.gel:40]
at PRU_PINMUX_Config() [PRU_CAPE.gel:25]
at PRU_Cape_Init()
If I try to connect the PRU core I obtain this message:
Error connecting to the target:
(Error -1170 @ 0x4A322000)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 6.0.407.3)
If I make a connection by the CD_DAP_DebugSS I'm able to read the address 0x4A322000 e 0x44e10990.
Running the test connection I don't have failoure.
What can I do in order to make this connection?
Thanks
Matteo