Team,
Can the AM572x Sitara DCAN controller support MilCAN-B?
I understand that part of the MilCAN-B recommendation is handle by the SW and we seem that we have Third party that provide MilCAN stack:
https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/198314/804508#804508
But from the CAN controller there are some specific requirements to be met. The specific interest is the following requirement from the MilCAN specification:
3.2.10 Link Layer Flow Control – Compulsory
The ‘overload’ frame of the ISO11898 CAN standard should never be invoked by the LLC
sub-layer of a device’s CAN controller. CAN controllers should be selected such that they
can accommodate the maximum level of bus activity.
Can the DCAN controller be setup to support this?
Thanks in advance,
Anthony