Tool/software: Linux
Hi All,
I have two AM5728 boards one EVM and another one is custom Boards.
We know that evm has PCIE with on board external clock for PCIe ref clock. In my custom board there is no on board external clock for PCIe ref clock.
Presently I am using Linux SK v.03.02 and running the default u-boot, kernel and devicetree for both the board with a minor modification in board.c file in u-boot.
int board_fit_config_name_match(const char *name)
{
if (board_is_x15() && !strcmp(name, "am57xx-beagle-x15"))
return 0;
else if (board_is_am572x_evm() && !strcmp(name, "am57xx-beagle-x15"))
return 0;
else if (board_is_am572x_idk() && !strcmp(name, "am572x-idk"))
return 0;
else if (board_is_am571x_idk() && !strcmp(name, "am571x-idk"))
return 0;
else
return 0;//-1; modified
}
The "lspci" command in Linux console for TI Am5728 board is giving the following message
am57xx-evm login: root
root@am57xx-evm:~# lspci
00:00.0 PCI bridge: Texas Instruments Device 8888 (rev 01)
But for custom board I am not getting any message for the same command "lspci".
Any help will be greatly appreciated.
Thanks
Srikanta