Tool/software: Linux
There is an external clk source for PCIe ref clk in AM5728 GP EVM.
I am using MLO, U-boot and rootfs obtained from Linux SDK v.03.02. for the EVM board.
when I use 'lspci' command in linux console it is giving the following message.
00:00.0 PCI bridge: Texas Instruments Device 8888 (rev 01)
Hi All,
After reading the CTRL_CORE_SMA_SW_6 register I am getting the following message.
root@am57xx-evm:~# devmem2 0x4a003c14 w
/dev/mem opened.
Memory mapped at address 0xb6f44000.
Read at address 0x4A003C14 (0xb6f44c14): 0x00000000
I have gone through the TRm and found the following statement in Table 18-1777. CTRL_CORE_SMA_SW_6:
17:16 PCIE_TX_RX_CONTROL PCIe RX and TX control of ACSPCIe.
0x0: ACSPCIe Power Down Mode
0x1: ACSPCIe TX Mode
0x2: ACSPCIe RX Mode
0x3: Reserved
So, as per TRM the CTRL_CORE_SMA_SW_6 register value at (17:16) bits position should be 0x2 as the PCIe ref clk in EVM is input.
Can anyone give some idea regarding this behaviour?
Thanks
Srikanta