Tool/software: Linux
Just received a new AM335x Evaluation module (NOT starter kit). P/N: TMDXEVM3358 Rev 1.6A.
Verified the dip switches were set in default position, inserted factory SD card and tried to boot, got the following message on the serial port console:
CCCCCCCC
U-Boot SPL 2011.09 (Apr 08 2012 - 18:29:14)
Texas Instruments Revision detection unimplemented
Incorrect magic number in EEPROM
read_eeprom() failure
From other posts, the fix seems to be fixing an I2C EEPROM that wasn't programmed properly. Directions seem to apply to the Starterkit, but some postings indicate it also applies to the Evaluation module. I created an SD card
Booted EVM with this card, ran the memory programming / show configurations and have this:
1. Show Configurations
2. Edit Configurations
3. Any Other Key to Cancel
Enter Your Choice : 1
**********************************************
TMDXEVM3358-SK Board
******** Reading From ID MEMORY *****
Header in ID-MEMORY LSB: 0xAA
Header in ID-MEMORY : 0x55
Header in ID-MEMORY : 0x33
Header in ID-MEMORY MSB: 0xEE
BOARD NAME IN ID-MEMORY : A33515BB
VERSION NUMBER : 1.6A
SERIAL NUMBER : 36154P160256
Configurations : SKU#01
**********************************************
Tried to boot with the factory SD card and still get the read_eeprom error.
How can I correct this?