I'm trying to see if it is possible to have EtherCAT + Gigabit Ethernet (1 port) + Display using the Pin Mux Tool. I'm having trouble getting started though because of ambiguity over what pins are actually needed for EtherCAT. Looking at the AM437x IDK as a reference, it looks like I should be choosing MDIO_PRUSS1 and MII_PRUSS1 as the interfaces. However, there's also an item in Pin Mux Tool called ECAT_PRUSS1, which seems like it should surely be the thing right?! However, adding ECAT_PRUSS1 even as the very first item leads to a bunch of conflicts.
Can someone please help me understand how Pin Mux Tool should be configured to represent an EtherCAT Slave?