Hi,
I'm trying to emulate an SD card (long story) -- heres the diagram:
I'm fairly sure I need an FPGA but I was wondering if its possible to use the AM335x?
SDIO on the AM335x is most likely host only, can't be used as a slave what about the GPIOs? They can't toggle faster than 208 MHz (which is necessary for the highest speeds SDR104, 104 MB/s, 208 MHz), what about slower speeds like 100 MHz or 50 MHz?