This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Linux/AM5728: PLL clock setting for 3 video outputs

Part Number: AM5728

Tool/software: Linux

Hi Expert,

We have a board with 3 video outputs on am5728.

dss channel lcd1, vout1 to our hdmi encoder 1.
dss channel tv, hdmi to tpd12s.
dss channel lcd2, vout2 to out hdmi encoder 2.

However, I can't configure clk src correctly.
Dss-pll driver can't set M4 and M6 clock both active.

How to configure video output src clk?
Should I use video2 PLL?

My psdk version is 3.02.05.

Regards,
Hugo


=====================DSS clock script===================
Dumps internal clocks and muxes of DSS

CTRL_CORE_DSS_PLL_CONTROL (0x4a002538) = 0x00000282
video1 PLL : Enabled
video2 PLL : Disabled
HDMI PLL : Enabled
DSI1_A_CLK mux : DPLL Video1
DSI1_B_CLK mux : DPLL Video1
DSI1_C_CLK mux : DPLL Video1

DSS_CTRL (0x58000040) = 0x00011001
2: LCD1 clk switch : DSI1_A_CLK
3: LCD2 clk switch : DSI1_B_CLK
10: LCD3 clk switch : DSS clk
1: func clk switch : DSS clk
13: DPI1 output : LCD1

DSS_STATUS (0x5800005C) = 0x01409282

DSI_CLK_CTRL (0x58004054) = 0x80004001

CM_DSS_CLKSTCTRL (0x4A009100) = 0x00040F03

CM_DSS_DSS_CLKCTRL (0x4A009120) = 0x00001702

========================================================
Register dump for DPLL video1
|----------------------------|
| Address (hex) | Data (hex) |
|----------------------------|
| 0x58004300 | 0x00000018 |
| 0x58004304 | 0x00002603 |
| 0x58004308 | 0x00000000 |
| 0x5800430C | 0x000DEC4E |
| 0x58004310 | 0x00E06008 |
| 0x58004314 | 0x0000000B |
| 0x58004318 | 0x00000000 |
| 0x5800431C | 0x00000000 |
| 0x58004320 | 0x00000000 |
|----------------------------|
Details for DPLL video1
PLL status : Locked
M4 hsdiv(1) : inactive
M5 hsdiv(2) : inactive
M6 hsdiv(3) : Active
M7 hsdiv(4) : inactive

PLL_REGM = 1782
PLL_REGN = 39
M4 DIV = 0
M6 DIV = 11
M7 DIV = 0

Clock calculations (DPLL video1)
sysclk = 20000000
DCO clk = sysclk * 2 * REGM / (REGN + 1) = 1782000000
M4clk (clkcout1) = DCO clk / (M4 DIV + 1) = 0
M6clk (clkcout3) = DCO clk / (M6 DIV + 1) = 148500000
M7clk (clkcout4) = DCO clk / (M7 DIV + 1) = 0

========================================================
Register dump for DPLL hdmi
|----------------------------|
| Address (hex) | Data (hex) |
|----------------------------|
| 0x58040200 | 0x00000018 |
| 0x58040204 | 0x00000003 |
| 0x58040208 | 0x00000000 |
| 0x5804020C | 0x0003600E |
| 0x58040210 | 0x00602004 |
| 0x58040214 | 0x00001400 |
| 0x58040218 | 0x00000000 |
| 0x5804021C | 0x00000000 |
| 0x58040220 | 0x00040000 |
|----------------------------|
Details for DPLL hdmi
PLL status : Locked
M4 hsdiv(1) : inactive
M5 hsdiv(2) : inactive
M6 hsdiv(3) : inactive
M7 hsdiv(4) : inactive

PLL_REGM = 432
PLL_REGN = 7
M4 DIV = 0
M6 DIV = 0
M7 DIV = 0
PLL_REGM2 = 1
PLL_REGM_F = 1
PLL_SD = 5
HDMI_SSC_CONFIGURATION1(should be zero) 0x00000000
HDMI_SSC_CONFIGURATION2(should be zero) 0x00000000

Clock calculations (DPLL hdmi)
sysclk = 20000000
CLKOUT = sysclk * REGM / (REGM2 * (REGN + 1)) = 1080000000

========================================================
Clock O/P of MUXes
DPLL PER H12 Output 192000000
CM_DIV_H12_DPLL_PER (0x4A00815C) = 0x00000204

DSI1_A_CLK : 0
DSI1_B_CLK : 148500000
DSI1_C_CLK : 148500000

DISPC_DIVISOR (0x58001804) = 0x00010001

2: LCD1 clk : 0
3: LCD2 clk : 148500000
10: LCD3 clk : 192000000
1: func clk : 192000000

LCD1 logic clk(/ 1 ) : 0 pix clk(/ 1 ) : 0
LCD2 logic clk(/ 1 ) : 148500000 pix clk(/ 1 ) : 148500000
LCD3 logic clk(/ 4 ) : 48000000 pix clk(/ 1 ) : 48000000

  • The video experts have been notified. They will respond here.

     

    Best Regards
    Biser
  • I add a patch to force M4/M6 active in function dss_pll_write_config_type_a now.
  • In reply to Hugo Hu:

    Yes, you should use PLL2.

    If the kernel is recent enough, in dpi.c there's dpi_get_clk_src_dra7xx(). It has a case for 'OMAP_DSS_CHANNEL_LCD2', which currently returns PLL1_3 by default, and PLL2_3 second. It should be swapped for your case.
  • In reply to manisha:

    I tried to swap PLL1_3 and PLL2_3 in dpi_get_clk_src_dra7xx().

    However, video2 PLL still inactive.

    How to enable video2 PLL in a general way?

  • In reply to Hugo Hu:

    Can you please share the diff of the changes you made and the linux kernel version you are using?

  • In reply to manisha:

    I just swap DSS_CLK_SRC_PLL1_3 and DSS_CLK_SRC_PLL2_3 in OMAP_DSS_CHANNEL_LCD2 case in function dpi_get_clk_src_dra7xx.

    My linux kernel is 4.4.32 base on psdk 3.02.05.

    static enum dss_clk_source dpi_get_clk_src_dra7xx(enum omap_channel channel)
    {
    	/*
    	 * Possible clock sources:
    	 * LCD1: FCK/PLL1_1/HDMI_PLL
    	 * LCD2: FCK/PLL1_3/HDMI_PLL (DRA74x: PLL2_3)
    	 * LCD3: FCK/PLL1_3/HDMI_PLL (DRA74x: PLL2_1)
    	 */
    	switch (channel) {
    	case OMAP_DSS_CHANNEL_LCD:
    	{
    		if (dss_pll_find_by_src(DSS_CLK_SRC_PLL1_1))
    			return DSS_CLK_SRC_PLL1_1;
    	}
    	case OMAP_DSS_CHANNEL_LCD2:
    	{
    		if (dss_pll_find_by_src(DSS_CLK_SRC_PLL1_3))
    			return DSS_CLK_SRC_PLL2_3;
    		if (dss_pll_find_by_src(DSS_CLK_SRC_PLL2_3))
    			return DSS_CLK_SRC_PLL1_3;
    	}
    	case OMAP_DSS_CHANNEL_LCD3:
    	{
    		if (dss_pll_find_by_src(DSS_CLK_SRC_PLL2_1))
    			return DSS_CLK_SRC_PLL2_1;
    		if (dss_pll_find_by_src(DSS_CLK_SRC_PLL1_3))
    			return DSS_CLK_SRC_PLL1_3;
    	}
    	default:
    		break;
    	}
    
    	return DSS_CLK_SRC_FCK;
    }

  • In reply to Hugo Hu:

    Hi Manisha,

    it's my mistake
    It can work with following change.

    Thank you again.


    case OMAP_DSS_CHANNEL_LCD2: { if (dss_pll_find_by_src(DSS_CLK_SRC_PLL2_1)) return DSS_CLK_SRC_PLL2_1; if (dss_pll_find_by_src(DSS_CLK_SRC_PLL1_3)) return DSS_CLK_SRC_PLL1_3; }

  • In reply to Hugo Hu:

    Hi manisha,

    Still got error after swap PLL2_3 & PLL1_3.

    In function dss_pll_write_config_type_a(),

    omapdss PLL error: cannot lock DSS DPLL.

    It cause dpi_set_mode fail.

    Do you have any comments or suggestions for this?

  • In reply to Hugo Hu:

    Suggested changes were tested at our end with kernel v4.9, and verified that both video plls getting enabled, and vsyncs at 60fps for both LCD outputs works fine.

    Did you also take care of the changes required in the dts configuration?

    Definitions for a second LCD in AM5 EVM dts file is needed , and set it to use the second port and then the dpi.c need to be changed as mentioned above. 

  • In reply to manisha:

    Hi Manisha,

    We will try it with kernel v4.9.

    I think our dts setting is ok.

    &dss {
    	status = "okay";
    	ports {
    		#address-cells = <1>;
    		#size-cells = <0>;
    
    		port@0 {
    			reg = <0>;
    			dpi_out_1: endpoint {
    				remote-endpoint = <&hdmi_encoder_1_in>;
    				data-lines = <24>;
    			};
    		};
    		port@1 {
    			reg = <1>;
    			dpi_out_2: endpoint {
    				remote-endpoint = <&hdmi_encoder_2_in>;
    				data-lines = <24>;
    			};
    		};
    	};
    };

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.