Tool/software: TI C/C++ Compiler
Hello:
I will save a test.ts file locally and use the following gstream command to display it properly.
gst-launch-1.0 -v filesrc location=test.ts ! queue ! tsdemux ! h264parse ! ducatih264dec ! waylandsink
I try to use C language to write,The image is not displayed when compiling execution.
Here is my source code:
I try to add the "--gst-debug = 4" parameter when executing, and the red section has an error message