I am working on a new board using the AM3358 to implement an audio driver using the McASP subsystem, and there are a couple of places where the technical reference manual (Literature number SPRUH73P) is not quite clear.
Specifically:
1) What is the purpose of the memory space shown in Table 2-1 McASP0 Data starting at 0x46000000 and McASP1 Data starting at 0x46400000? What is this connected to? How does data get from this space to the McASP?
2) In section 22.3.10.2.1 “AFIFO Data Transmission”, it states “If the host CPU writes to the Write FIFO, independent of a transmit DMA request, the WFIFO will accept host writes until full.”
Where is the AFIFO? At what address does the CPU write to to accomplish the above?
Thanks!