Tool/software: Linux
Trying to get the OpenCV examples to run on our AM5728 based platform. We are using the latest Arago release as a baseline.
When I follow the instructions here (your text render refuses to let me paste this as a link, it keeps rendering it as an image, so I put it in a code snippit):
processors.wiki.ti.com/.../OpenCV_AM57_Test_Instructions
I don't get the same results. Output from the instructions shows:
My output is:
CTEST_FULL_OUTPUT OpenCV version: 3.1.0 OpenCV VCS version: unknown Build type: release Parallel framework: tbb CPU features: neon
I don't see any OpenCL platform.
However, if I run the example in
/usr/share/ti/examples/opencl/platforms
I see that the OpenCL platform is detected properly:
Version: OpenCL 1.1 TI product version 01.01.09.1 (Oct 20 2016 15:48:24)
Vendor : Texas Instruments, Inc.
Profile: FULL_PROFILE
DEVICE: TI Multicore C66 DSP
Type : ACCELERATOR
CompUnits : 2
Frequency : 0.75 GHz
Glb Mem : 163840 KB
GlbExt1 Mem: 0 KB
GlbExt2 Mem: 0 KB
Msmc Mem : 1024 KB
Loc Mem : 128 KB
Max Alloc : 147456 KB
So maybe it has something to do with OpenCV? Is there some way of enabling debug output from OpenCV during run-time? Any other ideas?