Other Parts Discussed in Thread: AM3359
I am looking for an example to for the AM335x /MMC module to interface with the SD card.
My problem is the ACMD13 (SD Status) and the ACMD51 (SCR Register). These commands are supposed to have 512 bits (64 bytes) Block data sent to the host via the DATA register.
The commands are sent correctly without any error and the R1 response indicates that no error and the commands was successful.
However, when I read the SD_DATA (Offset 220h) register for the 512 bits block, it return all "0".
What did I do wrong, can you help?
Thanks
TRieu Pham