Tool/software: Linux
Hi all,I am working on a AM335x-SK board. SK stuck after print "Starting Kernel"First of all, I have tried the method introduced in http://processors.wiki.ti.com/index.php/Kernel_-_Common_Problems_Booting_Linux#Problem_.231_-_No_more_output_is_seen_on_the_console_after_.22Starting_Kernel....22, chanded console to ttyO0, ttyO2, ttyS2, but it doesn’t work.Also, I tried with board-support/prebuilt-images/ u-boot-spl.bin.am335x-evm, u-boot.img, zImage-am335x-evm.bin. The result is exactly the same as below.I download the am335-evm-SDK-3.3.0.4, and installed on Ubuntu1404 64bits, run setup.sh, (TFTP=1,NFS=1)Nothing is changed in Rules.make.
<am335x_evm.h>In am335x_evm.h, I modified the config_bootcommand as below:#define CONFIG_BOOTCOMMAND \"setenv autoload no; " \"setenv serverip 10.0.0.132; " \"dhcp; " \"tftp 0x82000000 10.0.0.132:uImage" \"bootm 0x82000000"Also, in .config, CONFIG_DEBUG_LL=y (but nothing printed after 'Starting kernel')All other files are kept the same as installed.I enter the SDK_install_dir, use the top makefile> make linux and copy the arch/arm/boot/zImage to /tftpboot, and use “mkimage -A arm -O linux -T kernel -C none -a 0x82000000 -e 0x820000000 -n "Linux kernel" -d zImage uImage ” to convert zimage to uimage.> make u-boot-spl and copy the u-boot.img and spl/u-boot-spl.bin to /tftpbootI use minicom to upload spl and u-boot file through xmodem and ymodem. u-boot download the uImage from my tftp, and shows following, then stuck.U-Boot 2016.05-00319-gcf14e63-dirty (May 25 2017 - 08:32:49 -0400)
CPU : AM335X-GP rev 1.0
Model: TI AM335x EVM-SK
Watchdog enabled
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Card did not respond to voltage select!
** Bad device mmc 0 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: eth0: ethernet@4a100000
Warning: usb_ether MAC addresses don't match:
Address in SROM is de:ad:be:ef:00:01
Address in environment is bc:6a:29:53:85:7b
, eth1: usb_ether
Press SPACE to abort autoboot in 2 seconds
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
BOOTP broadcast 2
DHCP client bound to address 10.0.0.133 (525 ms)
link up on port 0, speed 100, full duplex
Using ethernet@4a100000 device
TFTP from server 10.0.0.132; our IP address is 10.0.0.133
Filename 'uImage'.
Load address: 0x80008000
Loading: #################################################################
#################################################################
#################################################################
##########################################
1.9 MiB/s
done
Bytes transferred = 3474976 (350620 hex)
## Booting kernel from Legacy Image at 80008000 ...
Image Name: Linux kernel
Created: 2017-05-24 20:33:54 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3474912 Bytes = 3.3 MiB
Load Address: 82000000
Entry Point: 82000000
Verifying Checksum ... OK
Loading Kernel Image ... OK
Starting kernel ...
CCCCCCCCCIf I choose to download zImage and use bootz to run kernel, I got
Loading: #################################################################
#################################################################
#################################################################
##########################################
1.9 MiB/s
done
Bytes transferred = 3474912 (3505e0 hex)
Kernel image @ 0x80008000 [ 0x000000 - 0x3505e0 ]
Starting kernel ...
CCCCCCCCHere is the printenv output=> printenv
arch=arm
args_fit=setenv bootargs console=${console}
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUI
D=${uuid} rw rootfstype=${mmcrootfstype}
autoload== no
baudrate=115200
board=am335x
board_name=A335X_SK
board_rev=1.2B
board_serial=53124P197458
boot_a_script=load ${devtype} ${devnum}:${distro_bootpart} ${scriptaddr} ${prefi
x}${script}; source ${scriptaddr}
boot_efi_binary=load ${devtype} ${devnum}:${distro_bootpart} ${kernel_addr_r} ef
i/boot/bootarm.efi; if fdt addr ${fdt_addr_r}; then bootefi ${kernel_addr_r} ${f
dt_addr_r};elsebootefi ${kernel_addr_r} ${fdtcontroladdr};fi
boot_extlinux=sysboot ${devtype} ${devnum}:${distro_bootpart} any ${scriptaddr}
${prefix}extlinux/extlinux.conf
boot_fdt=try
boot_fit=0
boot_net_usb_start=usb start
boot_prefixes=/ /boot/
boot_script_dhcp=boot.scr.uimg
boot_scripts=boot.scr.uimg boot.scr
boot_targets=mmc0 legacy_mmc0 mmc1 legacy_mmc1 nand0 pxe dhcp
bootcmd=if test ${boot_fit} -eq 1; then run update_to_fit;fi;run findfdt; run in
it_console; run envboot; run distro_bootcmd
bootcmd_dhcp=run boot_net_usb_start; if dhcp ${scriptaddr} ${boot_script_dhcp};
then source ${scriptaddr}; fi
bootcmd_legacy_mmc0=setenv mmcdev 0; setenv bootpart 0:2 ; run mmcboot
bootcmd_legacy_mmc1=setenv mmcdev 1; setenv bootpart 1:2 ; run mmcboot
bootcmd_mmc0=setenv devnum 0; run mmc_boot
bootcmd_mmc1=setenv devnum 1; run mmc_boot
bootcmd_nand=run nandboot
bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi
bootcount=1
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootfile=boot.scr.uimg
bootm_size=0x10000000
bootpart=1:2
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
console=ttyO0,115200n8
cpu=armv7
devnum=1
devtype=mmc
dfu_alt_info_emmc=rawemmc raw 0 3751936
dfu_alt_info_mmc=boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x100 0x1
00;u-boot.img.raw raw 0x300 0x400;spl-os-args.raw raw 0x80 0x80;spl-os-image.raw
raw 0x900 0x2000;spl-os-args fat 0 1;spl-os-image fat 0 1;u-boot.img fat 0 1;uE
nv.txt fat 0 1
dfu_alt_info_nand=SPL part 0 1;SPL.backup1 part 0 2;SPL.backup2 part 0 3;SPL.bac
kup3 part 0 4;u-boot part 0 5;u-boot-spl-os part 0 6;kernel part 0 8;rootfs part
0 9
dfu_alt_info_ram=kernel ram 0x80200000 0xD80000;fdt ram 0x80F80000 0x80000;ramdi
sk ram 0x81000000 0x4000000
distro_bootcmd=for target in ${boot_targets}; do run bootcmd_${target}; done
dnsip=10.0.0.55
efi_dtb_prefixes=/ /dtb/ /dtb/current/
envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmc
dev};if run loadbootscript; then run bootscript;else if run loadbootenv; then ec
ho Loaded env from ${bootenvfile};run importbootenv;fi;if test -n $uenvcmd; then
echo Running uenvcmd ...;run uenvcmd;fi;fi;fi;
eth1addr=bc:6a:29:53:85:7b
ethact=ethernet@4a100000
ethaddr=bc:6a:29:53:85:7a
fdt_addr_r=0x88000000
fdtaddr=0x88000000
fdtcontroladdr=8ef282f8
fdtfile=am335x-evmsk.dtb
fileaddr=82000000
filesize=351048
findfdt=if test $board_name = A335BONE; then setenv fdtfile am335x-bone.dtb; fi;
if test $board_name = A335BNLT; then setenv fdtfile am335x-boneblack.dtb; fi; i
f test $board_name = BBG1; then setenv fdtfile am335x-bonegreen.dtb; fi; if test
$board_name = A33515BB; then setenv fdtfile am335x-evm.dtb; fi; if test $board_
name = A335X_SK; then setenv fdtfile am335x-evmsk.dtb; fi; if test $board_name =
A335_ICE; then setenv fdtfile am335x-icev2.dtb; fi; if test $fdtfile = undefine
d; then echo WARNING: Could not determine device tree to use; fi;
finduuid=part uuid mmc ${bootpart} uuid
fit_bootfile=fitImage.itb
fit_loadaddr=0x88000000
gatewayip=10.0.0.254
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${
loadaddr} ${filesize}
init_console=if test $board_name = A335_ICE; then setenv console ttyO3,115200n8;
else setenv console ttyO0,115200n8;fi;
ipaddr=10.0.0.197
kernel_addr_r=0x82000000
load_efi_dtb=load ${devtype} ${devnum}:${distro_bootpart} ${fdt_addr_r} ${prefix
}${efi_fdtfile}
loadaddr=0x82000000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
loadfit=run args_fit; bootm ${loadaddr}#${fdtfile};
loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
loadramdisk=load mmc ${mmcdev} ${rdaddr} ramdisk.gz
mmc_boot=if mmc dev ${devnum}; then setenv devtype mmc; run scan_dev_for_boot_pa
rt; fi
mmcboot=mmc dev ${mmcdev}; setenv devnum ${mmcdev}; setenv devtype mmc; if mmc r
escan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then if test
${boot_fit} -eq 1; then run loadfit; else run mmcloados;fi;fi;fi;
mmcdev=1
mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; the
n if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt}
= try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcrootfstype=ext4 rootwait
mtdids=nand0=nand.0
mtdparts=mtdparts=nand.0:128k(NAND.SPL),128k(NAND.SPL.backup1),128k(NAND.SPL.bac
kup2),128k(NAND.SPL.backup3),256k(NAND.u-boot-spl-os),1m(NAND.u-boot),128k(NAND.
u-boot-env),128k(NAND.u-boot-env.backup1),8m(NAND.kernel),-(NAND.file-system)
nandargs=setenv bootargs console=${console} ${optargs} root=${nandroot} rootfsty
pe=${nandrootfstype}
nandboot=echo Booting from nand ...; run nandargs; nand read ${fdtaddr} NAND.u-b
oot-spl-os; nand read ${loadaddr} NAND.kernel; bootz ${loadaddr} - ${fdtaddr}
nandroot=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048
nandrootfstype=ubifs rootwait=1
netargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${se
rverip}:${rootpath},${nfsopts} rw ip=dhcp
netboot=echo Booting from network ...; setenv autoload no; dhcp; run netloadimag
e; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdtaddr}
netloadfdt=tftp ${fdtaddr} ${fdtfile}
netloadimage=tftp ${loadaddr} ${bootfile}
netmask=255.255.255.0
nfsopts=nolock
partitions=uuid_disk=${uuid_gpt_disk};name=rootfs,start=2MiB,size=-,uuid=${uuid_
gpt_rootfs}
pxefile_addr_r=0x80100000
ramargs=setenv bootargs console=${console} ${optargs} root=${ramroot} rootfstype
=${ramrootfstype}
ramboot=echo Booting from ramdisk ...; run ramargs; bootz ${loadaddr} ${rdaddr}
${fdtaddr}
ramdisk_addr_r=0x88080000
ramroot=/dev/ram0 rw
ramrootfstype=ext2
rdaddr=0x88080000
rootpath=/export/rootfs
scan_dev_for_boot=echo Scanning ${devtype} ${devnum}:${distro_bootpart}...; for
prefix in ${boot_prefixes}; do run scan_dev_for_extlinux; run scan_dev_for_scrip
ts; done;run scan_dev_for_efi;
scan_dev_for_boot_part=part list ${devtype} ${devnum} -bootable devplist; env ex
ists devplist || setenv devplist 1; for distro_bootpart in ${devplist}; do if fs
type ${devtype} ${devnum}:${distro_bootpart} bootfstype; then run scan_dev_for_b
oot; fi; done
scan_dev_for_efi=setenv efi_fdtfile ${fdtfile}; if test -z "${fdtfile}" -a -n "$
{soc}"; then setenv efi_fdtfile ${soc}-${board}${boardver}.dtb; fi; for prefix i
n ${efi_dtb_prefixes}; do if test -e ${devtype} ${devnum}:${distro_bootpart} ${p
refix}${efi_fdtfile}; then run load_efi_dtb; fi;done;if test -e ${devtype} ${dev
num}:${distro_bootpart} efi/boot/bootarm.efi; then echo Found EFI removable medi
a binary efi/boot/bootarm.efi; run boot_efi_binary; echo EFI LOAD FAILED: contin
uing...; fi; setenv efi_fdtfile
scan_dev_for_extlinux=if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefi
x}extlinux/extlinux.conf; then echo Found ${prefix}extlinux/extlinux.conf; run b
oot_extlinux; echo SCRIPT FAILED: continuing...; fi
scan_dev_for_scripts=for script in ${boot_scripts}; do if test -e ${devtype} ${d
evnum}:${distro_bootpart} ${prefix}${script}; then echo Found U-Boot script ${pr
efix}${script}; run boot_a_script; echo SCRIPT FAILED: continuing...; fi; done
scriptaddr=0x80000000
serverip=10.0.0.55
soc=am33xx
spiargs=setenv bootargs console=${console} ${optargs} root=${spiroot} rootfstype
=${spirootfstype}
spiboot=echo Booting from spi ...; run spiargs; sf probe ${spibusno}:0; sf read
${loadaddr} ${spisrcaddr} ${spiimgsize}; bootz ${loadaddr}
spibusno=0
spiimgsize=0x362000
spiroot=/dev/mtdblock4 rw
spirootfstype=jffs2
spisrcaddr=0xe0000
static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
stderr=serial@44e09000
stdin=serial@44e09000
stdout=serial@44e09000
update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
usb_boot=usb start; if usb dev ${devnum}; then setenv devtype usb; run scan_dev_
for_boot_part; fi
usbnet_devaddr=de:ad:be:ef:00:01
vendor=ti
ver=U-Boot 2016.05-00319-gcf14e63-dirty (May 23 2017 - 10:40:38 -0400)
Environment size: 8792/131068 bytes<Rules.make><setup-minicom.sh>I browsed the e2e.ti forum, none of the related posts provide a workable solution.Could anybody help to figure out what’s the problem? If you need any other information, please let me know. Thank you very much.