Other Parts Discussed in Thread: TIDA-00299, AMIC110, TLK105, TLK110
Hi,
Is it possible that someone from TI clarify how to correctly connect Link/Activity LED and RXLINK (e.g. PR0_MII0_RXLINK) for the newest EtherCAT Firmware?
I have seen a lot of schematics with different approach. But I'm shure there is "best of" solution when using DP83822 PHY. E.g. TIDA-00299 schematic has no more connection from PHY's to the RXLINK signal in the PRU's (as far as I can see). Also from my point of view the DP83822 PHY is able to create the Link/Activity LED signal as needed by the EtherCAT Indicator ans Labeling Specification.
But what about Enhanced Link detection?
When I look into the PRU-ICSS EtherCAT Firmware API Guide (Wiki) I can see that a connection to the RXLINK (e.g. PR0_MII0_RXLINK) signals is still needed (recommended) for Enhanced Link detection.
If the Link LED signal from PHY needs to be used for RXLINK signal than one have to manually create the signal for the Link/Activity LED (e.g. by the EtherCAT application or stack)? Or is this done by some of the PRU GPIO's and the PRU firmware?
As you can see there is a lot of confusion about this.
Thanks and best regards,
Patrick