Hello,
I need to enable the PCI driver for the AM5718 board, in u-boot.
I used the u-boot provided in 04.00.00.04 sdk (last version available at this time).
When selection PCI driver in u-boot menuconfig, I have the following error during the compilation:
drivers/pci/built-in.o: In function `pci_init':
drivers/pci/pci.c:466: undefined reference to `pci_init_board'
A quick search of pci in boards/ti/ returns no occurrence.
It looks like there is no PCI initialization driver available in u-boot for TI boards.
Do you have a u-boot PCI driver available for am5718 board ? Is there a workaround in order to initialize PCI in u-boot?
I tried the u-boot from denx.de, and I have the same compilation problem.
Best regards