Hi !
Reading AM57xx reference manual (Rev I) - I found following note on page 6165:
"McASP1, McASP2, and McASP3, whose data port are accessible directly via L3_MAIN, do
not support FIFO/constant addressing modes. Incrementing transfers must be used instead."
Well, the idea of the data port is that I can access the serializers using the fifo with a single address.
As there are no other registers on the data port - the notation of incrementing transfers on it would be something I exclude.
So this basically means that data ports via L3_MAIN does not work !!!???
So the only way would be to use the edma with the CFG port without fifo.
In my case (only one channel) this would still be a non-incrementing access.
Or are there undocumented "shadow" addresses of the serializers at DATA port location !!??
rgds,
Wolfgang