This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/PROCESSOR-SDK-AM335X: Profinet Slave build problem

Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: SYSBIOS

Tool/software: TI-RTOS

Hello,    I am using CCS 7.2 and I am trying to build the AM335x PROFINET SLAVE (IRT).     I am having some type of version incompatibility problem between the TI.SYSBIOS.KNL package and the XDC TOOLS as reported during a build -- shown below.     The error is that the package "ti.sysbios.knl" is not compatible with the XDC tools used in the build.    One confusion is that the error message says to use XDCTools 3.50 or later and I believe that I am using 3.50.02.20.:

  

I have installed components as indicated in the TI directory:

And the CCS PROJECT properties showing the XDC TOOL VERSION and products:

Any help in resolving this would be greatly appreciated!!!

Mark