Other Parts Discussed in Thread: AM4379, AM4378
Hello,
We've successfully booted via UART and SD card however we now wish to boot via using USB client mode.
Under Linux we are receiving the following message in syslog...
[ 3365.929425] usb 1-1.4: new full-speed USB device number 15 using ehci-pci
[ 3366.022101] usb 1-1.4: not running at top speed; connect to a high speed hub
[ 3366.023727] usb 1-1.4: New USB device found, idVendor=0451, idProduct=6142
[ 3366.023729] usb 1-1.4: New USB device strings: Mfr=33, Product=37, SerialNumber=0
[ 3366.023731] usb 1-1.4: Product: AM43xx1.2
[ 3366.023732] usb 1-1.4: Manufacturer: Texas Instruments
[ 3371.021550] rndis_host 1-1.4:1.0: RNDIS init failed, -110
[ 3371.021564] rndis_host: probe of 1-1.4:1.0 failed with error -110
[ 3381.021526] rndis_wlan 1-1.4:1.0: RNDIS init failed, -110
[ 3381.021634] rndis_wlan: probe of 1-1.4:1.0 failed with error -110
[ 3957.285899] usb 1-1.4: USB disconnect, device number 15
I've not managed to find out exactly what this -110 error message means to understand why RNDIS is failing.
Using the AM437x GP EVM we get the same behaviour.
I am using Ubuntu 16.04 with NetworkManager installed. I have followed the TI instructions to configure ISC DHCP server and NetworkManager
What piece of information does the RNDIS_HOST module use to locate the configuration?
Daniel