Other Parts Discussed in Thread: TPS650250
Tool/software: Linux
Hi,
we are using Bealgbone black based custom board,
I was trying to get OPP by omapconf using command as mentioned below
./omapconf show pwst
But OPP column says “NOT FOUND”
However when I run same command on beaglbone black I get the values.
I have attached file which has output of above command from both the boards.
Actually I wanted to verify eMMC clock. I get clock speed as 52Mhz from sysfs, from TRM it is fixed at 48Mhz but it also mentions 48Mhz @ OPP50
I am not sure if that OPP is for eMMC or OPP of am335x.
So now I want to know OPP so that we can understand what is the max eMMC clock we set for AM3352.
# cat /sys/kernel/debug/mmc1/ios
clock: 52000000 Hz
vdd: 20 (3.2 ~ 3.3 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 3 (8 bits)
timing spec: 1 (mmc high-speed)
signal voltage: 0 (3.30 V)
Thank you,
Regards,
Ankur
=================================================================================================================================================================== custom board =================================================================================================================================================================== # ./omapconf show pwst OMAPCONF (rev v1.73-19-gbe8626b built Wed Sep 13 10:18:44 EDT 2017) HW Platform: Generic AM33XX (Flattened Device Tree) AM3352 ES2.1 GP Device (UNKNOWN performance ZCE package (600MHz)) UNKNOWN POWER IC UNKNOWN AUDIO IC SW Build Details: Build: release_details_get(): could not open /etc/issue.net file?! Version: UNKNOWN Kernel: Version: 3.12.10-005-ts-armv7l Author: ankur@ankur-HP-Z440-Workstation Toolchain: gcc version 4.8.3 (Timesys 20170124) Type: #1 Date: Tue Sep 12 16:36:33 EDT 2017 |---------------------------------------------------------------------------------------------------------------------------------------------------------------| | OMAP Power Status | |---------------------------------------------------------------------------------------------------------------------------------------------------------------| | Voltage Domain | Power Domain | Clock Domain | Module Status | | Name | OPP | Name | Curr. | Target | Name | Status | Name | Rate (MHz) | Idle | Standby | |---------------------------------------------------------------------------------------------------------------------------------------------------------------| | VDD_CORE | NOT FOUND | WKUP | OFF | OFF | L4WKUP | Running | L4_WKUP_INTERCONNECT | 100.000 | Full ON | | | | | | | |------------------------------------------------------------------------------------------------| | | | | | | WKUP_L3_AON | Running | DEBUGSS | 200.000 | In Transition | Functional | | | |-------------------------------------------------------------------------------------------------------------------------------| | | | GFX | ON | ON | GFX_L3 | Gated | GFX | 100.000 | Disabled (NO ACCESS) | | | | |-------------------------------------------------------------------------------------------------------------------------------| | | | PER | ON | ON | L4_SLOW | Running | L4_PER_INTERCONNECT | 100.000 | Full ON | | | | | | | |------------------------------------------------------------------------------------------------| | | | | | | L3_SLOW | Running | L3_MAIN1_INTERCONNECT | 100.000 | Full ON | | | | | | | |------------------------------------------------------------------------------------------------| | | | | | | L3_FAST | Running | L3_MAIN2_INTERCONNECT | 200.000 | Full ON | | | | | | | | | | EMIF4 | 200.000 | Full ON | | | | | | | | | | PHY_EMIF | 400.000 | | | | | | | | |------------------------------------------------------------------------------------------------| | | | | | | L4_FAST | Running | L4_FAST_INTERCONNECT | 200.000 | Full ON | | |---------------------------------------------------------------------------------------------------------------------------------------------------------------| | VDD_MPU | NOT FOUND | MPU | ON | ON | MPU | Running | MPU | 550.000 | Full ON | | |---------------------------------------------------------------------------------------------------------------------------------------------------------------| =================================================================================================================================================================== Beaglebone Black =================================================================================================================================================================== ./omapconf show pwst OMAPCONF (rev v1.73-19-gbe8626b built Wed Sep 13 10:18:44 EDT 2017) HW Platform: Generic AM33XX (Flattened Device Tree) AM3359 ES2.0 GP Device (UNKNOWN performance ZCZ package (1.0GHz)) Error: I2C Read failed Error: I2C Read failed Error: I2C Read failed TPS65217C ES1.2 Error: I2C Read failed UNKNOWN AUDIO IC SW Build Details: Build: Version: _____ _____ _ _ Kernel: Version: 4.4.41-gf9f6f0db2d Author: ankur@ankur-HP-Z440-Workstation Toolchain: gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) Type: #1 PREEMPT Date: Tue Jun 6 10:25:28 EDT 2017 |---------------------------------------------------------------------------------------------------------------------------------------------------------------| | OMAP Power Status | |---------------------------------------------------------------------------------------------------------------------------------------------------------------| | Voltage Domain | Power Domain | Clock Domain | Module Status | | Name | OPP | Name | Curr. | Target | Name | Status | Name | Rate (MHz) | Idle | Standby | |---------------------------------------------------------------------------------------------------------------------------------------------------------------| | VDD_CORE (1.125V) | OPP100 | WKUP | OFF | OFF | L4WKUP | Running | L4_WKUP_INTERCONNECT | 100.000 | Full ON | | | | | | | |------------------------------------------------------------------------------------------------| | | | | | | WKUP_L3_AON | Running | DEBUGSS | 200.000 | In Transition | Functional | | | |-------------------------------------------------------------------------------------------------------------------------------| | | | GFX | ON | ON | GFX_L3 | Running | GFX | 100.000 | Full ON | Functional | | | |-------------------------------------------------------------------------------------------------------------------------------| | | | PER | ON | ON | L4_SLOW | Running | L4_PER_INTERCONNECT | 100.000 | Full ON | | | | | | | |------------------------------------------------------------------------------------------------| | | | | | | L3_SLOW | Running | L3_MAIN1_INTERCONNECT | 100.000 | Full ON | | | | | | | |------------------------------------------------------------------------------------------------| | | | | | | L3_FAST | Running | L3_MAIN2_INTERCONNECT | 200.000 | Full ON | | | | | | | | | | EMIF4 | 200.000 | Full ON | | | | | | | | | | PHY_EMIF | 400.000 | | | | | | | | |------------------------------------------------------------------------------------------------| | | | | | | L4_FAST | Running | L4_FAST_INTERCONNECT | 200.000 | Full ON | | |---------------------------------------------------------------------------------------------------------------------------------------------------------------| | VDD_MPU (0.950V) | OPP50 | MPU | ON | ON | MPU | Running | MPU | 300.000 | Full ON | | |---------------------------------------------------------------------------------------------------------------------------------------------------------------|