Hi
I am trying to get my custom board up and running but it fails to start from the SD-card. My custom board is based on the BBB board with only minor modifications. Boot configuration is the same as the BBB.
I have followed the AM335x bringup tips and all voltage and frq (also CLKOUT1 after enabling it) is ok as well as PORZ.
When powering up the board I can measure data on the CLK pin of the SDcard and if a valid sdcard is inserted there is also data on data0 but it dies out short time after and nothing more happens. Uart0 is not available for measureing so I can't check if there is a "C" output. The SD-card has been tested on a BBB so I know for sure that it is working.