Tool/software: TI-RTOS
Hi,
I check with the following SDK and evaluation board.
SDK version : ti-processor-sdk-rtos-AM57xx 04.01.00.06
EVM board : TMDXIDKAM5728 rev 1.3B
There is a problem that does not start when using the MLO(prebuild and build) of the SDK in the version of this board.
Case the same MLO is used in the old version IDK(rev 1.1A), it can start normally.
It also starts normally on linux
Is there information on something about it?
Best Regards,
Shigehiro Tsuda