Part Number: BEAGLEBK
Tool/software: Linux
Hi,
I am unable to connect through SSH to Beaglebone Black booted from SD card with the am335x-evm-linux-04.01.00.06 image. I have noticed this error message during the booting process:
[FAILED] Failed to start Start USB gadget.
See 'systemctl status gadget-init.service' for details.
The result of the "systemctl status gadget-init.service" is the following:
[[0;1;31m●[[0m gadget-init.service - Start USB gadget
Loaded: loaded (/lib/systemd/system/gadget-init.service; enabled; vendor preset: enabled)
Active: [[0;1;31mfailed[[0m (Result: exit-code) since Tue 2017-09-26 21:31:46 UTC; 59s ago
Process: 573 ExecStart=/usr/bin/gadget-init.sh [[0;1;31m(code=exited, status=1/FAILURE)[[0m
Main PID: 573 (code=exited, status=1/FAILURE)
Sep 26 21:31:44 am335x-evm systemd[1]: Starting Start USB gadget...
Sep 26 21:31:44 am335x-evm gadget-init.sh[573]: SERIAL_NUMBER = 2016BBBK0C83
Sep 26 21:31:44 am335x-evm gadget-init.sh[573]: PRODUCT = BeagleBoneBlack
Sep 26 21:31:44 am335x-evm gadget-init.sh[573]: host_addr = 88:C2:55:4C:2C:DB
Sep 26 21:31:46 am335x-evm gadget-init.sh[573]: ifconfig: SIOCGIFFLAGS: No such device
Sep 26 21:31:46 am335x-evm gadget-init.sh[573]: ifconfig: SIOCSIFADDR: No such device
Sep 26 21:31:46 am335x-evm systemd[1]: [[0;1;39mgadget-init.service: Main process exited, code=exited, status=1/FAILURE[[0m
Sep 26 21:31:46 am335x-evm systemd[1]: [[0;1;31mFailed to start Start USB gadget.[[0m
Sep 26 21:31:46 am335x-evm systemd[1]: [[0;1;39mgadget-init.service: Unit entered failed state.[[0m
Sep 26 21:31:46 am335x-evm systemd[1]: [[0;1;39mgadget-init.service: Failed with result 'exit-code'.[[0m
I also include below the later messages from the boot, in case they can shed more light.
I am using Windows 10.
Thank you and regards
Adam
[FAILED] Failed to start Start USB gadget.
See 'systemctl status gadget-init.service' for details.
[ 25.879576] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 25.985904] usbcore: registered new interface driver usbfs
[ 25.985967] usbcore: registered new interface driver hub
[ 25.986083] usbcore: registered new device driver usb
[ 26.391188] using random self ethernet address
[ 26.412558] using random host ethernet address
[ 26.417082] using host ethernet address: 88:C2:55:4C:2C:DB[ 26.515110] usin g random self ethernet address
[ 26.577386] using random host ethernet address
[ 26.628137] using host ethernet address: 88:C2:55:4C:2C:DB[ 26.688222] usb0 : HOST MAC 88:c2:55:4c:2c:db
[ 26.749153] usb0: MAC 22:0c:05:e9:1d:09
[ 26.906892] Mass Storage Function, version: 2009/09/11
[ 26.912078] LUN: removable file: (no medium)
[ 26.987692] LUN: removable read only file: /dev/mmcblk0p1
[ 27.026340] Number of LUNs=1
[ 27.069773] g_multi gadget: Multifunction Composite Gadget
[ 27.121656] g_multi gadget: g_multi ready
[ 27.168175] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 27.294194] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 27.299592] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numbe r 1
[ 27.420549] g_multi gadget: high-speed config #1: Multifunction with RNDIS
[ 27.511557] ti-pruss 4a300000.pruss: creating PRU cores and other child platf orm devices
[ 27.547155] irq: no irq domain found for /ocp/pruss_soc_bus@4a326000/pruss@4a 300000/intc@4a320000 !
[ 27.554258] irq: no irq domain found for /ocp/pruss_soc_bus@4a326000/pruss@4a 300000/intc@4a320000 !
[ 27.843504] hub 1-0:1.0: USB hub found
[ 27.886456] hub 1-0:1.0: 1 port detected