Other Parts Discussed in Thread: SYSBIOS
Hi,
I am evaluating AM3359 for industrial application and planning to use SYS/BIOS for RTOS purpose.
Initially I download the IND SDK ( am335x_sysbios_ind_sdk_01.01.03.03) and try to run “ethernetip_adapter” project.
During compilation I am getting below error
“This project was created using a version of XDCtools that is not currently installed: 3.23.0.14.eng. Please install the XDCtools of this version, or migrate the project to one of the supported versions.”
I tried refactor to upgrade XDCtools, but still we are getting below error regarding XDC tool
“xdc.tools.configuro: Error: Can't find the platform package 'ti.platforms.evmAM3359'. TI platforms are no longer shipped as part of XDCtools (C:\ti\xdctools_3_50_03_33_core). Please ensure you are either using a pre-3.30 version of XDCtools or you have added a product that includes your platform support along the path ';C:\ti\xdctools_3_50_03_33_core/packages'. Check that this path names a directory containing the necessary platform support and that the platform name is properly spelled.”
After that I created my own project and import C file of “ethernetip_adapter” project and try to compile it, now XDC version error is solve but there is error for no definition of MMUInit and UTILsDetectBoardType
Function. I searched in SDK folder, but there is no difinition for these function.
Kindly help me regarding above problem or provide link of example project.
I am using version number 7.3.0.00019 and XDC tool version is 3_50_03_33_core.
thanks