Other Parts Discussed in Thread: TPS65910,
Tool/software: Linux
Hello TI Team,
In SDK v04.02.00.09 and I do the 1st ifconfig to start ethernet, it will be failed. And then I do 2nd ifconfig, it will be work. The relative message is as below.
ifconfig eth0 up
[ 21.385132] net eth0: initializing cpsw version 1.12 (0)
[ 21.460245] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 21.466684] cpsw 4a100000.ethernet: ALE Table size 1024
[ 21.492279] net eth0: phy "4a101000.mdio:00" not found on slave 0, err -19
[ 21.503293] cpts ptp bc clkid 0
[ 21.520252] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
/ # ifconfig eth0 down
/ # ifconfig eth0 up
[ 29.511081] net eth0: initializing cpsw version 1.12 (0)
[ 29.516480] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 29.523000] cpsw 4a100000.ethernet: ALE Table size 1024
[ 29.532809] TI DP83867 4a101000.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=4a101000.mdio:00, irq=-1)
[ 29.548066] cpts ptp bc clkid 0
[ 29.563772] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready