Tool/software: Linux
Hello Everyone,
We have purchased a Beagle-bone Black board for development purpose to prepare our custom product based on AM3358 processor. During the development we are facing issue in Firmware flashing using USB Flash Drive on Beagle-bone Black. While flashing new Firmware using USB Flash drive showing below error.
Running uenvcmd ...
resetting USB...
USB0: Port not available.
** Bad device usb 0 **
reading logo.bin
90672 bytes read in 13 ms (6.7 MiB/s)
reading zImage
8197016 bytes read in 464 ms (16.8 MiB/s)
reading am335x-boneblack.dtb
63897 bytes read in 10 ms (6.1 MiB/s)
Kernel image @ 0x80100000 [ 0x000000 - 0x7d1398 ]
## Flattened Device Tree blob at 81000000
Booting using the fdt blob at 0x81000000
Loading Device Tree to 8ffed000, end 8ffff998 ... OK
Note: We have one pen-drive (with full details as below) is working fine for Flashing Firmware but other USB Flash Drive does not work with the same board.
[ +0.000007] usb 1-2: Product: STEC USB 2.0
[ +0.000005] usb 1-2: Manufacturer: STEC
[ +0.000006] usb 1-2: SerialNumber: 86AA0E00E88B08C9
Thanks & Best Regards;
Nikunj Patel