Tool/software: Linux
Hi,
I am using AM572x EVM and have problem connecting to C66x using JTAG. I am able to connect and load the code to all cores with JTAG. But when I have Linux running on A15, when I tried to connect to C66 cores, JTAG always complains that 'the core is held in reset'. I am using the standard image for SD card created by Linux SDK. And I believe there are codes for both C66s that are loaded into the C66 by the boot loader.
Here is my question: How can I connect ONLY to C66 using JTAG while Linux is running on A15?
Thanks