This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3354: FIQ interrupts

Part Number: AM3354

Tool/software: Linux

Hello

AM3354BZCZAI00 This CPU is now used, the original use is GPIO3_21 interrupt.

Because the project has relatively high requirements for interruption, it is almost impossible to lose the interruption. With this ordinary IRQ interrupt, about 2000 interrupts will lose about 4 or so.

Mapping this IRQ interrupt to the FIQ interrupt should not cause the interrupt to be lost.

I would like to ask this CPU can use FIQ interrupt? There is currently no way to find out on the Internet.

Do you have any relevant examples?

--Thanks and Best Regards